Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design Configuring UART0
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 2 replies
  • Subscribers 359 subscribers
  • Views 512 views
  • Users 0 members are here
Related

Configuring UART0

Former Member
Former Member over 10 years ago

Hi,

I an running eCos on zedboard. By default eCos is configured to UART 0. I would like to configure UART 0 (similar to UART 1) and get the output on host machine through terminal (putty).

In vivado for zedboard, UART 0 is set to EMIO as IO.

1. I would like to know how this EMIO output can be accessed via terminal (putty console) in host.

2. Can we access UART 0 output via USB-OTG port of zedboard.

Thanks in advance

  • Sign in to reply
  • Cancel
Parents
  • bhfletcher
    0 bhfletcher over 10 years ago
    1.   UART 0 may connect to EMIO by default, but you could also manipulate it to connect it to the PS Pmod. EMIO is also valid, but then you have to provide constraints to specify which pins to use (the PL Pmods would be a good choice).
       
        This gives you a UART at the SoC pins, which is not enough to connect to a PC. You also need a transceiver. I suggest you look at USB-UART or RS232 Pmods.
         
    2.   No

    Honestly, you'd save yourself a whole lot of time by figuring out how to configure eCos for UART 1.

     

    Bryan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Reply
  • bhfletcher
    0 bhfletcher over 10 years ago
    1.   UART 0 may connect to EMIO by default, but you could also manipulate it to connect it to the PS Pmod. EMIO is also valid, but then you have to provide constraints to specify which pins to use (the PL Pmods would be a good choice).
       
        This gives you a UART at the SoC pins, which is not enough to connect to a PC. You also need a transceiver. I suggest you look at USB-UART or RS232 Pmods.
         
    2.   No

    Honestly, you'd save yourself a whole lot of time by figuring out how to configure eCos for UART 1.

     

    Bryan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Children
  • Former Member
    0 Former Member over 10 years ago in reply to bhfletcher

    Thanks Bryan Fletcher

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer