Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design ZedBoard Rev.C + AD-FMCMOTCON2-EBZ
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 360 subscribers
  • Views 582 views
  • Users 0 members are here
Related

ZedBoard Rev.C + AD-FMCMOTCON2-EBZ

100mikro
100mikro over 9 years ago

Hello everyone,

since 2 months I am in the world of ZedBoard.

I always got problems when I wanted to download the bitstreams per USB-UART interface and run the external simulation from Matlab per TCP/IP interface.

I need to try several times until one successful bitstream download or one successful external mode simulation.

 

I firstly contacted with Mathworks for this reason and it turned out, my ZedBoard Rev.C has also some hardware issues with itself. After reading the ZedBoard errata Rev.C, I did a hardware fix on USB-UART interface, but there is another issue for "SD Card Clock Series Termination", a 40 Ohm to 60 Ohm resistor in series needed on SDIO clock pin. I do not think I can fix it by my side. So this issue of SDIO clock pin will not be fixed.

 

My quesition or consideration: by downloading the bitstreams and by running external simulation, the SD card will be written too. So could the SDIO clock issue be a big problem by ZedBoard Rev. C, that the reading or writting files from SD card sometimes corruptted.

 

By the way, I also used the board AD-FMCMOTCON2-EBZ board for motor control from analog devices. Except this connection issue on ZedBoard Rev.C, everything works well.

Could this issue be solved with ZedBoard Rev.D or later?

Windows 10 64bit is my operation system + Matlab R2017a + Vivado 2016.2

  • Sign in to reply
  • Cancel
Parents
  • 100mikro
    0 100mikro over 9 years ago

    I just want to upload an updated info.

    1, this issue above was only for the case, if I wanted to download the bitstream to Zedboard with USB-UART interface.

    2, the drive for USB-UART, Cypress has been installed correctly and I also tried to re-install it, but it did not help.

    3, so SD card read/writing should not be the cause.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • 100mikro
    0 100mikro over 9 years ago

    I just want to upload an updated info.

    1, this issue above was only for the case, if I wanted to download the bitstream to Zedboard with USB-UART interface.

    2, the drive for USB-UART, Cypress has been installed correctly and I also tried to re-install it, but it did not help.

    3, so SD card read/writing should not be the cause.