Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design Optimizing Boot Time
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 5 replies
  • Subscribers 359 subscribers
  • Views 825 views
  • Users 0 members are here
Related

Optimizing Boot Time

Former Member
Former Member over 12 years ago

Iu2019m trying to minimize bare metal boot time using QSPI flash on a Zedboard, Rev C.  Using a scope, Iu2019ve verified the QSPI SCLK is running at 100 MHz.  At that speed, the boot time should be less than 100 msec (Boot ROM + FSBL + PL + PS) but Iu2019m measuring close to 600 msec.  Monitoring the CS signal on the flash device I see what appears to be many 8 clock cycles of data transfer then a pause of 100 nsec after each one.  In addition to these pauses is a periodic delay of around 6 usec and a several pauses in the 50 msec range.  What are these delays?  Is there something in the FSBL that can be adjusted to remove them?
tt
Thanks for your help!
Clay

  • Sign in to reply
  • Cancel
Parents
  • Former Member
    0 Former Member over 12 years ago

    Hi,
    could u share how did u measure 600msec whole boot time?

    According to avnet doc it should be...

    As 100MHz QSPI Flash device throughput of up to 50MB/s)


    Parameter Time (ms)
    Power Ramp 50
    PLL Lock 0.05
    PS Image Load (5MB) 100
    PL Image Load (5MB) 100
    Total Boot Time 250.05

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Former Member
    0 Former Member over 12 years ago

    Hi,
    could u share how did u measure 600msec whole boot time?

    According to avnet doc it should be...

    As 100MHz QSPI Flash device throughput of up to 50MB/s)


    Parameter Time (ms)
    Power Ramp 50
    PLL Lock 0.05
    PS Image Load (5MB) 100
    PL Image Load (5MB) 100
    Total Boot Time 250.05

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
No Data