Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design Zedboard FMC: External Clock
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 360 subscribers
  • Views 511 views
  • Users 0 members are here
Related

Zedboard FMC: External Clock

Former Member
Former Member over 10 years ago

Hi all

I'm realy new to the Zedboard, but it looks very interesting.

An so I've a question: for a school-project I need an external clock in the PL (a teacher told me that this isn't realy complex). Unfortunately there isn't any SMA connector for an external clock (like it was at the spartan-3 boards). I read in this forum, that there are 2 possibile clock inputs on the FMC connector (FMC_CLK0_P / FMC-CLK0_N and FMC_CLK1_P / FMC-CLK1_N). So I could use them. Is there any existing fmc-board that I can use? I found several for ethernet, da and ad conversion, but nothing so simple.

And if there isn't one, what is the exactly connecter I've to use for a selfmade-board?

I hope you could help me...
thank you very much
best regards.

  • Sign in to reply
  • Cancel
Parents
  • Former Member
    0 Former Member over 10 years ago

    Hi Kevin

    Thank you very much for your fast response.

    Yes, I need a off-board clock source.
    The Debug-Board looks great. Nearly what I've looked for. But with this restrictions I can live.

    Are there any problem, if I use the single ended clock (the P one) as the clock input (82MHz) and and the negative one as normal IO (signal 100kHz to 8.2MHz with defined phase to the 82MHz)? It would be nice, if I can use both sma-connector independ.

    The best would be if there is a board with 4 sma connectors, but I can live with only 2 (independ).

    Best regards,
    Patrick

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Former Member
    0 Former Member over 10 years ago

    Hi Kevin

    Thank you very much for your fast response.

    Yes, I need a off-board clock source.
    The Debug-Board looks great. Nearly what I've looked for. But with this restrictions I can live.

    Are there any problem, if I use the single ended clock (the P one) as the clock input (82MHz) and and the negative one as normal IO (signal 100kHz to 8.2MHz with defined phase to the 82MHz)? It would be nice, if I can use both sma-connector independ.

    The best would be if there is a board with 4 sma connectors, but I can live with only 2 (independ).

    Best regards,
    Patrick

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
No Data