Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design ZedBoard Choice to a Radar design
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 1 reply
  • Subscribers 358 subscribers
  • Views 276 views
  • Users 0 members are here
Related

ZedBoard Choice to a Radar design

e14 Contributor
e14 Contributor over 12 years ago

Hi,
Please i would like to select the best suitable xilinx platform for a Radar implementation.
My specs:
Sampling freq : 250 Mhz.
ADC resolution : 14 bits.
I already implemented this project using the high speed A/D K7 (Kc705) board, there was an FMC150 ADC/DAC card and a target reference design which i used to invoke the Radar signal processing blocks with this TRD.
Now i need to implement the Radar signal processing blocks on a dsp ( processor) not an FPGA. I searched a lot till i came up to the best solution i know which is the ZedBoard as it contains an ARM processor and the interface holds the LPC for the FMC150 card.
In another meaning, i need to take the sampled bits and do the processing using a dsp core, so i don't have to care about the ADC interface.
I would like to have an installation like described above or if you got something better,please advise me.


Thanks alot.

  • Sign in to reply
  • Cancel
  • bhfletcher
    0 bhfletcher over 12 years ago

    The MicroZed with a MicroZed FMC Carrier would be another option. If you need a Zynq larger than the 7020, then you could look at the Zynq MMP system.

     

    Bryan