Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design linux kernel make module option
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 361 subscribers
  • Views 673 views
  • Users 0 members are here
Related

linux kernel make module option

100aditya
100aditya over 9 years ago

Dear sir

 

  I am working on Zedboard and trying to build mine kernel. So here is mine snippet of mine script:-

echo -e "\e[0;32m---- Build kernel -----------\e[0m" source ~/architech_sdk/architech/zedboard/toolchain/environment-nofs make LOADADDR=0x8000 uImage

echo -e "\e[0;32m---- Build modules ---\e[0m"

make modules

 

I am having the .config file for mine Zedboard.The problem is this moment i am calling make modules it is giving me a lot of option and asking to put yes or no for each of one. I am very new to Linux and i do not know about those options. What is way out??

 

Regards

Aditya

 
  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 9 years ago

    Aditya,

    I think your problem with the kernel configuration may be that you skipped the step of setting up a default configuration file for the target.  Without this, menuconfig will ask you to specify all the different possible options, as you have found.  If you first create a default-configuration file, most of the options for a basic boot are pre-defined, and then you only change the options you care about (maybe none).

    You can see an example of how this works for a kernel build on the ADI wiki:

    https://wiki.analog.com/resources/tools-software/linux-drivers/platforms/zynq

    The line you are looking for is:  make zynq_xcomm_adv7511_defconfig

    That file is specific for the ADI Ubuntu kernel and activates various drivers used there. You can look in the kernel you have under:

    /arch/arm/configs/

    I think you can find a zedboard defconfig file in there.

    Ron

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 9 years ago

    Aditya,

    I think your problem with the kernel configuration may be that you skipped the step of setting up a default configuration file for the target.  Without this, menuconfig will ask you to specify all the different possible options, as you have found.  If you first create a default-configuration file, most of the options for a basic boot are pre-defined, and then you only change the options you care about (maybe none).

    You can see an example of how this works for a kernel build on the ADI wiki:

    https://wiki.analog.com/resources/tools-software/linux-drivers/platforms/zynq

    The line you are looking for is:  make zynq_xcomm_adv7511_defconfig

    That file is specific for the ADI Ubuntu kernel and activates various drivers used there. You can look in the kernel you have under:

    /arch/arm/configs/

    I think you can find a zedboard defconfig file in there.

    Ron