Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design Zedboard AXI DMA Problem
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 1 reply
  • Subscribers 357 subscribers
  • Views 367 views
  • Users 0 members are here
Related

Zedboard AXI DMA Problem

Former Member
Former Member over 11 years ago

I have a Zynq design that uses the AXI DMA module. However I find that the DMA transfer is not starting.

To start the DMA transfer I do the following things

Write the MM2S_CR to set RS to 1
Write the MM2S_SA to be the source address
Write the MM2S_LENGTH to be the length in bytes of the data
my addresses for the registers are
0x40400000 (base / MM2SCR)
0x40400018 = base + 18h = MM2S_SA
0x40400048 = base + 28h = MM2S_LENGTH

However it seems that when I try to set the values of the registers MM2S_SA and LENGTH with Xil_Out32(addr, value) the setting doesn't work per inspection through XMD.

Following this I tried to set the values in XMD with mrd/mwr and they aren't changing that way either.

Any advice/help would be greatly appreciated.
Thank you



  • Sign in to reply
  • Cancel
  • Former Member
    0 Former Member over 11 years ago

    Solved, Since scatter gather was still enabled (It was supposed to be disabled) those registers aren't used.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer