Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design Data via RS232 or GPIB(IEC-625-Bus)?
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 1 reply
  • Subscribers 359 subscribers
  • Views 397 views
  • Users 0 members are here
Related

Data via RS232 or GPIB(IEC-625-Bus)?

e14 Contributor
e14 Contributor over 12 years ago

Hi guys,

I wanted to control my function Generator and lab power supply which have GPIB and RS232 Interfaces.

Is there a way to use the Zedboard the way I could send data via one of the two Interfaces?

thx in advance

  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Maxim makes an RS232 PMOD module that can be plugged into the ZedBoard PMOD connectors. I have used one to drive the signals from the 2nd Zynq PS UART. You can add additional axi_uart cores in the Zynq programmable logic as well. Due to the width of this module you could probably only fit 3 on a ZedBoard

     

    http://datasheets.maximintegrated.com/en/ds/MAX3232PMB1.pdf

     

    Avnet does have them in stock:

     http://avnetexpress.avnet.com/store/em/EMController?action=products&catalogId=500201&storeId=500201&N=0&langId=-1&slnk=b&term=MAX3232PMB1&hrf=http%3A%2F%2Fwww.em.avnet.com%2Fen-us%2Fdesign%2Fdrc%2FPages%2FMaxim-Pmod-Compatible-Plug-In-Peripheral-Modules.aspx

     

    -Gary