Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design LVDS transmit and receive
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 360 subscribers
  • Views 1121 views
  • Users 0 members are here
Related

LVDS transmit and receive

roopasampath
roopasampath over 9 years ago

My customer is trying to use the Zedboard to generate LVDS out Bank 34 at 2.5V and then loop it back into the FPGA to test their receiver.  The receiver side locks to the transmit clock just fine (ISERDES and IDELAY primitives being used) but they noticed the data lines don't look to be giving a full LVDS swing voltage like the clocks are.  Any ideas on what could be happening?  They checked to be sure an IBUFDS is being used on the receiver and transmitter and termination has been enabled.

Any suggestions would be appreciated.

Regards,

Roopa

  • Sign in to reply
  • Cancel
Parents
  • drozwood90
    0 drozwood90 over 9 years ago

    Hi there,

    How is the lack of voltage swing being detected?
    Are they using a scope?  Logic Analyzer?  A custom LVDS circuit or analyzer?
    Remember that unless you are doing a m-LVDS setup, you cannot rely on reading the LVDS lines direct u2013 especially in parallel to the existing circuit.  Care MUST be taken to measure this.

    Is the customer not seeing data, although the clock is OK?  How are they detecting that the clock is OK, but no data?  Have they tried to place a canned pattern in, such as CACA, something that you can EASILY detect?

    --Dan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • drozwood90
    0 drozwood90 over 9 years ago

    Hi there,

    How is the lack of voltage swing being detected?
    Are they using a scope?  Logic Analyzer?  A custom LVDS circuit or analyzer?
    Remember that unless you are doing a m-LVDS setup, you cannot rely on reading the LVDS lines direct u2013 especially in parallel to the existing circuit.  Care MUST be taken to measure this.

    Is the customer not seeing data, although the clock is OK?  How are they detecting that the clock is OK, but no data?  Have they tried to place a canned pattern in, such as CACA, something that you can EASILY detect?

    --Dan