Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design DDR0V75 Supply Bypassing
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 359 subscribers
  • Views 433 views
  • Users 0 members are here
Related

DDR0V75 Supply Bypassing

e14 Contributor
e14 Contributor over 12 years ago

On sheet 14 of the zedboard schematic, why is DDR0V75 bypassed to DDR1V5 instead of ground?

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Hi, if bypassing were done so that DDR0V75 remains at half of DDR1V5, wouldn't it still make sense to have bypass caps between DDR0V75 and ground, and also DDR0V75 and DDR1V5? I don't see how bypassing to only DDR1V5 instead of ground helps maintain the half-value point.

    Both the ZC702 board and microzed board bypass it to ground, and that makes more sense to me. It might be possible to get rid of the DDR0V75 termination voltage altogether depending on the board layout, but I haven't looked into it. Just wondering if there was a specific reason why the Zedboard is different from the ZC702, because I'm referencing both of them for a design I'm working on.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Hi, if bypassing were done so that DDR0V75 remains at half of DDR1V5, wouldn't it still make sense to have bypass caps between DDR0V75 and ground, and also DDR0V75 and DDR1V5? I don't see how bypassing to only DDR1V5 instead of ground helps maintain the half-value point.

    Both the ZC702 board and microzed board bypass it to ground, and that makes more sense to me. It might be possible to get rid of the DDR0V75 termination voltage altogether depending on the board layout, but I haven't looked into it. Just wondering if there was a specific reason why the Zedboard is different from the ZC702, because I'm referencing both of them for a design I'm working on.