Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design DDR0V75 Supply Bypassing
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 359 subscribers
  • Views 430 views
  • Users 0 members are here
Related

DDR0V75 Supply Bypassing

e14 Contributor
e14 Contributor over 12 years ago

On sheet 14 of the zedboard schematic, why is DDR0V75 bypassed to DDR1V5 instead of ground?

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Yes, you're right, bypass to 1.5 V sees full fluctuation, to ground sees none, and for half the fluctuation you need to do both. But since this is termination, not a reference level, I don't think that matters that much anyway.

    Another possibility is the termination currents are better handled by the supply than the ground. The termination currents would go back on dedicated power bus to the 1.5V supply and not cross talk to other devices via a shared ground.  But this is just another small design subtlety.

    Again, I don't think it's critical, especially if you have a good ground. The proof is that boards have gone both ways and work fine.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Yes, you're right, bypass to 1.5 V sees full fluctuation, to ground sees none, and for half the fluctuation you need to do both. But since this is termination, not a reference level, I don't think that matters that much anyway.

    Another possibility is the termination currents are better handled by the supply than the ground. The termination currents would go back on dedicated power bus to the 1.5V supply and not cross talk to other devices via a shared ground.  But this is just another small design subtlety.

    Again, I don't think it's critical, especially if you have a good ground. The proof is that boards have gone both ways and work fine.