Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design Help for program and boot from QSPI
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 359 subscribers
  • Views 1064 views
  • Users 0 members are here
Related

Help for program and boot from QSPI

Former Member
Former Member over 12 years ago

Currently I am working on Zedboard.

For test purpose, I created a small project and programmed through JTAG (J17). It is working with the bit file.

After that, I created MCS file through IMPACT. Then I would like to program the QSPI and like to boot through QSPI directly.

IMPACT can detect zynq7000_arm and xc7Z020. And it seems that I can only add SPI/BPI at zynq7000_arm. But when I added QSPI, it shows warning the warning message:

"The "data width" you assigned is x0 but the PROM file (.mcs) is generated in a x1 mode. ..."

It seems I can keep on program by ignore this message. But the problem it never work as booting from QSPI.

I ever tried to read back the MCS file and it is only 3K. This is not matching the MCS file I programmed into (~10M). It seems the problem is that the QSPI didn't program correctly.

Anyone has suggestion on it?

Thanks a lot,

  • Sign in to reply
  • Cancel
  • Former Member
    0 Former Member over 12 years ago

    hi,
    I have the same problem. I managed to program the QSPI flash correctly (at least, the was no error message), but I cant boot the zedboard from the QSPI.

    Did you solve it?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 11 years ago in reply to Former Member

    Did you solve this? I am stuck in the same problem ... however when I boot from SD, everything is OK.

    By the way, I am using Vivado.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 11 years ago

    Here is how my solution.
    http://svenand.blogdrive.com/archive/201.html

    Sven

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer