Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design LPDDR2 with Zynq 7000
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 5 replies
  • Subscribers 360 subscribers
  • Views 2016 views
  • Users 0 members are here
Related

LPDDR2 with Zynq 7000

e14 Contributor
e14 Contributor over 11 years ago

Hi ZedBoard Forum,

i want to create a new design with the Zynq 7000 series(7020). On the new PCB should be a LPDDR2 Memory.

As a reference Design i am using the ZedBoard.

The DDR Memory Controller has the following Limitations,see (TRM UG585,p.294):

Maximum Total Memory Density 1 GB
Total Data Width (bits) 16, 32
Component Data Width (bits) 8, 16, 32
Maximum Ranks 1
Maximum Row Address (bits) 15
Maximum Bank Address (bits) 3

So my question is, can i use the following LPDDR2 with a memory Single Channel S4 Configuration (256 Meg x 32)?

http://www.micron.com/parts/dram/mobile-ddr2-sdram/mt42l256m32d2lk-18-wt

I think the Ranks per channel can be a problem, am i right ?


Thanks for your help!

hb_zed



  • Sign in to reply
  • Cancel
Parents
  • bhfletcher
    0 bhfletcher over 11 years ago

    If you want to make your life easier, I suggest you use one of the parts built into the ZYNQ7 PS configuration menu. I see these two in 2015.1:

     

    MT42L64M32D1KL-25

    MT42L128M16D1KL-25

     

    The part you reference will be a problem for the Zynq PS built-in DDR controller due to the rank. Zynq only has 1 CS, and the part you show requires 2.

     

    I also suggest you search the Xilinx forums. A search for "Zynq LPDDR2" returns 50 discussions.

    http://forums.xilinx.com/t5/forums/searchpage/tab/message?filter=labels&q=zynq+lpddr2

     

    Bryan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • bhfletcher
    0 bhfletcher over 11 years ago

    If you want to make your life easier, I suggest you use one of the parts built into the ZYNQ7 PS configuration menu. I see these two in 2015.1:

     

    MT42L64M32D1KL-25

    MT42L128M16D1KL-25

     

    The part you reference will be a problem for the Zynq PS built-in DDR controller due to the rank. Zynq only has 1 CS, and the part you show requires 2.

     

    I also suggest you search the Xilinx forums. A search for "Zynq LPDDR2" returns 50 discussions.

    http://forums.xilinx.com/t5/forums/searchpage/tab/message?filter=labels&q=zynq+lpddr2

     

    Bryan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to bhfletcher

    Thanks Bryan for your fast answer.

    So that means i could use the 128 Meg x 32 configuration right ?

    I also thinking about to connect the 2 CS wire in the Layout, do you think it is possible ?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • bhfletcher
    0 bhfletcher over 11 years ago in reply to e14 Contributor

    You could use the 128M x 32, or you could use two of the 256M x 16, but that complicates your layout.

     

    Connecting the two CS wires in layout will not allow the controller/memory to work properly.

     

    Bryan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 9 years ago in reply to bhfletcher

    I have a  LPDDR 2  (KEP04GSC-MABDMKAM1C32),the fsbl of zedboard give the message below:

    PCW Silicon Version : 3.0
    Xilinx First Stage Boot Loader
    Release 2014.3  Dec 19 2016-11:16:20
    DDR_INIT_FAIL
    FSBL Status = 0xA007
    In FsblHookFallback function

    how can I solve the problem?