Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design Zedboard Power Issue
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 359 subscribers
  • Views 1005 views
  • Users 0 members are here
Related

Zedboard Power Issue

100emile
100emile over 8 years ago

Hi,

I'm working on the zedboard. Since today, I was able to run the Linux demo and the hardware seemed to work fine. But now, when I power up the board, the LD13 just don't light on. When I plug the micro-USB cable in J17 and J14 my PC still recognize the board so I assume that some power is delivered but I can't run the linux demo neither program the FPGA. I think that the issue is that PG-ALL is at a strange 0.7 V level. Jumpers are good. I suspected something wrong near IC29-LM339M:

V_IN1+ = 1V

V_IN1- = 0.9V

V_OUT1 = 5V **As expected

 

V_IN2+ = 1V

V_IN2- = 0.9V

V_OUT2 = 0.7 V ** I will have expected 5V

 

V_IN3+ = 0.7 V

V_IN3- = 2.97 V

V_OUT3 = 0 V ** Because V_OUT2 = 0.7V

 

V_IN4+ = 0.6 V

V_IN4- = 0.58 V

V_OUT4 = 0.7V ** On the same net of V_OUT2

 

As I will expected 5V at V_OUT2 for PG-ALL, I think that the problem might be a the comparator. Some of you experience this before? What did go wrong? Could someone confirm the voltages on IC29-LM339M?

 

Thank you

  • Sign in to reply
  • Cancel
Parents
  • daisy
    0 daisy over 4 years ago

    How did you solve the problem afterward?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • daisy
    0 daisy over 4 years ago

    How did you solve the problem afterward?