Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design ZEDBoard FMC TCK Tristate buffer enable
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 1 reply
  • Subscribers 360 subscribers
  • Views 436 views
  • Users 0 members are here
Related

ZEDBoard FMC TCK Tristate buffer enable

e14 Contributor
e14 Contributor over 11 years ago

I think I found an error in the IC1B Tri-state buffer for the TCK JTAG signal routing to the FMC port.

The enable signal for the part B of the 74LCX125BQX Tri-state buffer has a pin# of 1 on the schematic.  This is incorrect.  This gate should have its enable on pin#4.

I think I have traced this on the PCB as well, so I don't think this is just an error on the schematic.  It is hard to check this for sure without the Altium file.  Pin 4 is floating as far as I can tell.   But could someone check this for me.

Thx

  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    Hi psydway,

    You are correct, it is a bug in the schematic and pin 4 is indeed floating on the board. The buffer seems to be enabled and passing the JTAG clock independent of the presence of an FMC add-on. Although the behavior with a floating OE in undefined, on all the boards we looked at the buffer was enabled. If you are having functional issues, you might want to jump wire pins 1 and 4.