Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design Accidentally short circuited 12V, is it repairable?
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 359 subscribers
  • Views 321 views
  • Users 0 members are here
Related

Accidentally short circuited 12V, is it repairable?

e14 Contributor
e14 Contributor over 13 years ago

Hello!

I just accidentally short circuited 12V pin on the FMC card to ground. Now the 12V pin shows about 2.5V while on and 4.25V while off. No lights on the board are lit. How would I go about figuring out what has broke? Do you think it is repairable?

  • Sign in to reply
  • Cancel
  • bhfletcher
    0 bhfletcher over 13 years ago

    The FMC 12V is supplied from the ZedBoard through net VU12V0.  The source of VU12V0 is the power switch attached directly to the AC/DC wall supply.  A 5A fuse (http://www.te.com/catalog/pn/en/F21397-000) is in the path, so maybe you got lucky and just blew the fuse.  Check the voltage coming out of your wall supply to see if it is 12V.  If not, then you need to replace it.  If the wall supply is delivery 12V, then check the fuse F5.

     

    Bryan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to bhfletcher

    Yes, it seems to be the fuse!

    Many thanks! Your help is very much appreciated!