Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design AES-FMC-HDMI-CAM-G Tutorials
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 360 subscribers
  • Views 748 views
  • Users 0 members are here
Related

AES-FMC-HDMI-CAM-G Tutorials

slm130430
slm130430 over 9 years ago

Hello - My project is to do video processing with the Zedboard Zynq-7000 SoC. We have implemented our convolution architecture using Vivado 2016.2 and are now focusing on the video I/O portion. To facilitate HDMI input and output, we ordered the AES-FMC-HDMI-CAM-G module. Here is the link for the module:

https://products.avnet.com/shop/en/ProductDisplay?storeId=715839035&catalogId=10001&langId=-1&productId=3074457345628965509

1. In attempting the tutorials on the product page, we are encountering a number of issues. First question: Can we use ANY HDMI (unencrypted) source with this module, or does it only support certain cameras? I note the product page identifies two "related parts": (a) the AES-CAM-ON-P1300C-G ON Semiconductor PYTHON-1300-Color Camera, and (b) the AES-CAM-TOSH-1080P-G Toshiba Industrial 1080P60 Camera Module. We are not using either of these cameras, nor do we want to. 

2. Are there any in-depth tutorials for the FMC-HDMI-CAM-G module in addition to the ones linked to on the product page?

Many thanks, Stuart

  • Sign in to reply
  • Cancel
  • albertabeef
    0 albertabeef over 9 years ago

    Stuart,

    Any non-encrypted DVI or HDMI video source should work with the FMC-HDMI-CAM's HDMI input.

    Regards,

    Mario.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • slm130430
    0 slm130430 over 9 years ago in reply to albertabeef

    Hi Mario - Thanks for the reply! I've come across a number of tutorials using the FMC IMAGEON module. For example, there is a good HDMI pass-through tutorial that we'd like to start with.

    I understand that the IMAGEON module is obsolete, however, will the FMC-HDMI-CAM module work with the old IMAGEON tutorials?  

    Many thanks, Stuart

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • albertabeef
    0 albertabeef over 9 years ago

    Stuart,

    Yes, the FMC-HDMI-CAM is backwards compatible with the FMC-IMAGEON for the I2C interfaces and HDMI interfaces.

    The only difference resides in the camera interface, which are different for both modules.

    Regards,

    Mario.