Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design Execute a model on target
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 3 replies
  • Subscribers 360 subscribers
  • Views 666 views
  • Users 0 members are here
Related

Execute a model on target

e14 Contributor
e14 Contributor over 10 years ago

Hello,
I want to execute a model on the FPGA of Zedboard. I've created a VHDL model in Simulink but, when I execute it on the target, I receive the follow message. I don't know what is the problem. I think I need to install some software in Zedboard but, when I tried to do any change, the system doesn't save the changes. So, I don't know how to solve it. can anyone to help me? Any idea?
Thanks!


/arm-xilinx-linux-gnueabi-gcc -c -O0 -march=armv7-a -mcpu=cortex-a9 -mfpu=neon -mfloat-abi=softfp -DMODEL=BuckConverter10 -DNUMST=1 -DNCSTATES=0 -DHAVESTDIO -DONESTEPFCN=1 -DTERMFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=0 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=0 -D__MW_TARGET_USE_HARDWARE_RESOURCES_H__ -DARM_PROJECT -DRT -DSTACK_SIZE=64 -DONESTEPFCN=1 -DTERMFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=0 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=0 -DARM_PROJECT -DRT -DSTACK_SIZE=64 -DMODEL=BuckConverter10 -DNUMST=1 -DNCSTATES=0 -DHAVESTDIO -IC:/Xilinx/14.7/ISE_DS/ISE/BuckConverter10_ert_rtw -IC:/Xilinx/14.7/ISE_DS/ISE -IC:/Users/Rocio/Documents/02 PFC/04 Simulaciones/Pruebas/Buck Converter -IC:/PROGRA~1/MATLAB/R2014b/extern/include -IC:/PROGRA~1/MATLAB/R2014b/simulink/include -IC:/PROGRA~1/MATLAB/R2014b/rtw/c/src -IC:/PROGRA~1/MATLAB/R2014b/rtw/c/src/ext_mode/common -IC:/PROGRA~1/MATLAB/R2014b/rtw/c/ert -IC:/MATLAB/SupportPackages/R2014b/xilinxzynq7000ec/toolbox/target/supportpackages/zynq/@slCustomizer/../include -IC:/MATLAB/SupportPackages/R2014b/armcortexa/toolbox/target/supportpackages/arm_cortex_a/include -IC:/PROGRA~1/MATLAB/R2014b/toolbox/target/codertarget/rtos/inc -o "BuckConverter10.c.o" "C:/Xilinx/14.7/ISE_DS/ISE/BuckConverter10_ert_rtw/BuckConverter10.c" "/arm-xilinx-linux-gnueabi-gcc" no se reconoce como un comando interno o externo, programa o archivo por lotes ejecutable. gmake: *** [BuckConverter10.c.o] Error 1

  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 10 years ago +1 verified
    Hello Matt, I've solved my problem. I have two installation of ISE Design Suite, 14.4 and 14.7. I knew that Zedboard need the version 14.7 but I had the oldest installed. I've uninstalled the oldest version…
  • mbrown
    0 mbrown over 10 years ago

    In order to get familiar with how the MathWorks Zynq flow works using External Mode, I would recommend starting with this tutorial:

     

    http://www.mathworks.com/help/hdlcoder/examples/getting-started-with-hardware-software-codesign-workflow-for-xilinx-zynq-platform.html?s_tid=srchtitle

     

    Once you have this working, you'll have confidence that the tools and hardware are configured correctly.

     

    /Matt

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    Hello Matt,

    thank you for you response. I executed this example and I've executed again, and I saved it in the SD card too. Everything is OK.

    I have a problem when I execute 'Generate Software Interface Model' step, with hdlcode_led_blinking and other models. If I don't check 'Add IP core device driver to Linux Model', I pass the step but, if I mark it, I can't pass it and the system response : 'Failed Error while executing SSH command: 'cp -f /mnt/devicetree.dtb /mnt/originalDeviceTree'. Please check IP Address, user name and password options.'.

    I copied devicetree.dtb file in originalDeviceTree in the system, I've executed again my model and the follow message is about don't find 'dtc -V' command. I tried to install but the result wasn't OK either.

    If I execute the step in my model or in hdlcoder_data_capture model,  without check 'Add IP core device driver to Linux Model', I pass the step and the follows, but I can't execute it in model external because I have the first error that I commented.

    I don't know if I've explained everything OK, I'm sorry for my English.

    I've found the original boot image of the SD card because I thought my problem was in its contents, like the boot is from the SD card... But I think it's OK because I've change all files with the original...

    What do you think?

     

    Tanks!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    Hello Matt,

    I've solved my problem. I have two installation of ISE Design Suite, 14.4 and 14.7. I knew that Zedboard need the version 14.7 but I had the oldest installed. I've uninstalled the oldest version and I've reconfigured everything (Matlab, ISE and Zedboard) and I've updated Zedboard target too. Now, I can execute everything without problems. Everything run OK.

    Thank you very much for your help.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Reject Answer