Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design PS will dynamically configure PL by PCAP
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 1 reply
  • Subscribers 359 subscribers
  • Views 506 views
  • Users 0 members are here
Related

PS will dynamically configure PL by PCAP

Former Member
Former Member over 12 years ago

Hi,

It seems to me that it is possible to dynamically configure PL through PCAP via PS..i.e. I would store the.bin file ( converted .bit which actually contains the PL logic) in DDR SDRAM and now with the help of PS, I would dump those .bin in PL and my would get full configured..

I found the source (http://forums.xilinx.com/t5/Embedded-Processor-System-Design/How-to-use-PCAP-to-config-the-PL-in-zynq/td-p/280230).

For simplicity let , I have and.bin, or.bin and nand.bin 3 simple PL logic..So now I wrote a program that if I give input 1 via UART, it would dump and logic , if 2 then or and if 3 then nand..but things not working as I wished..
I load and.bin in DDR via XMD then it dumped board via PCAP..but when I load or.bin in DDR via xmd at different address only Or.bin get dumped , and.bin might have erased..

any soln that how it could work flawlessly..
thanls

  • Sign in to reply
  • Cancel
  • Former Member
    0 Former Member over 12 years ago

    What's the size range for your bin files ?
    Why dont you implement a function to dump DDR content in some segment to the UART so you can be sure whether files were downloaded correctly or not and detect potential data collision !

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer