Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design SDIO for Windows 7
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 9 replies
  • Subscribers 360 subscribers
  • Views 1059 views
  • Users 0 members are here
Related

SDIO for Windows 7

e14 Contributor
e14 Contributor over 12 years ago

Good morning from Germany,
I would like to know wheter if there is any library / API for SDIO device on Zynq. We are developing a Bare Metal Software which has to log some data on SD card, through SDIO interface.
Thank you in advance,
Michel

  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Hi

    I have not done anything with SDIO, but have made a fully working bare metal Vivado project that allows you to work with an SD card in SPI mode. It uses the 'FatFs' libraries available here -
    http://elm-chan.org/fsw/ff/00index_e.html

    Enabling GPIO in the PS block, you can then communicate through MIO pins 40-47, which are the pins in the SD slot on the Zedboard. (I am sure this is not the best way to do this, but it works!)

    I made the modifications to the 'generic' version of the FatFs library and have stuck the C files here so you can have a look
    http://personal.strath.ac.uk/kenneth.barlee/zed_posts/fatfs_sd.zip

    Kenny

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Hi, Kenny.

    It's great!!
    Does "Enabling GPIO" means that pin40-47 should be GPIO not SD0?
    I will try.

    Thank you.
    Sam

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Hi, Kenny.

    It's working!!
    Thank you for your idea!!

    sam

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to e14 Contributor

    ...haha - glad I could help!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to e14 Contributor

    For anyone else reading this - yes, set the MIO pins 40-47 to be GPIO

    K

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    HI, Kenny.

    Could this library create a binary file and write in binary format?

    Sean

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to e14 Contributor

    Hi Sean,

    Yes I am sure it probably could. If you look at the main.c file though, you will see that functions have been created that allow for files + folders to be created, and char strings to be written to them.

    If you are wanting to log binary values to a file I would suggest something along the lines of

    //stackoverflow.com/questions/111928/is-there-a-printf-converter-to-print-in-binary-format
    const char *byte_to_binary(unsigned long x)
    {
    tstatic char binary[32];
    tbinary[0]='0';
    tint z;
    tfor (z = 134217728; z > 0; z >>= 1)
    t{
    ttstrcat(binary,((x & z) == z)?"1":"0");
    t}
    treturn binary;
    }

    void main(void)
    {
         ....

    t//BINARY VALUE
    tint bin = 0b010101010101;

    t//CREATE NEW FILE
    tprintf("
    create a new file (binary.txt)");
    trc = f_open(&Fil, "BINARY.TXT", FA_WRITE | FA_CREATE_ALWAYS);
    tif (rc) die(rc);

    t//WRITE TO NEW FILE
    tprintf("
    write binary data");
    tchar buffer[33];
    tsprintf(buffer,"%s
    ",byte_to_binary(bin));
    trc = f_write(&Fil, *buffer, strlen(buffer), &bw);
    tif (rc) die(rc);

    t//CLOSE NEW FILE
    tprintf("
    close the file");
    trc = f_close(&Fil);
    tif (rc) die(rc);

    t...
    }
    (note - not tested!)

    ...rather than writing binary commands. If you want to do that though, I guess you would have to manipulate some of the files in the background. Have not done it myself so could not comment!

    Kenny

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to e14 Contributor

    HI, Kenny.

    It does work! Thank you for answering!

    Sean

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • ttkee
    0 ttkee over 8 years ago

    Hi  

    I am getting this error  10 = FR_WRITE_PROTECTED = The physical drive is write when everytime I run the application. 

    I used diskpart to to disable write protection, but I still get the same error.