Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design Zedboard + PmodAD5
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 1 reply
  • Subscribers 360 subscribers
  • Views 639 views
  • Users 0 members are here
Related

Zedboard + PmodAD5

e14 Contributor
e14 Contributor over 9 years ago

Hi,

I'm trying to make PmodAD5 work with a Zedboard by using Vivado 2016.2 (can also use earlier versions if needed). Digilent has a nice wiki pages to use Pmods with Zedboard, especially for using Pmod IPs:

https://reference.digilentinc.com/learn/programmable-logic/tutorials/pmod-ips/start

In this tutorial, however, there is no PmodAD5, and there reference design linked from Digilent product page to AD also has the implementation example for Xilinx ISE 14.4:

https://wiki.analog.com/resources/fpga/xilinx/pmod/ad7193

Nevertheless I tried to combine the information I could find to start with a ZYNQ7 Processing System with AXI Quad SPI IP.  (I managed to work with that way with a MAXIM Pmod temperature sensor).

But I got stuck at some point as to communicating with PmodAD5 device. After HW and SW implementation I am getting the following output on the UART:

Status Register: 0x0

Mode Register: 0x0

(The second one should be different than 0x0 according to documentation)

Is there someone out there tried PmodAD5 with Zedboard who could help me?

 

Since this is my first post I tried to explain the overall status. If there are questions specific to the project I am more than happy give additional info.

Thanks.

  • Sign in to reply
  • Cancel
  • jafoste4
    0 jafoste4 over 9 years ago

    Hello Analoghb,

    I see you have already posted this question over on the Digilent forum.

    https://forum.digilentinc.com/topic/2871-pmodad5-with-zedboard/#comment-10113

    In my research I was unable to find much in the way of examples or reference designs. However, I did find this post over on the Digilent forum that seems comprehensive which may be of help!

    https://forum.digilentinc.com/topic/153-pmod-ad5/

    --Josh