Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design GEAR MOTOR interfacing with zedboard in vhdl
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 1 reply
  • Subscribers 359 subscribers
  • Views 384 views
  • Users 0 members are here
Related

GEAR MOTOR interfacing with zedboard in vhdl

e14 Contributor
e14 Contributor over 11 years ago

hi,

i am trying to interface modelcraft gear motor with zedboard i am having problem while coding it n do i need a driver board.Any help would be appreciated

Regards
Annu shah
Heidelberg University

  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    As discussed in your previous post http://zedboard.org/content/zedboard-run-motors you can directly connect digital servo motors like those found in RC cars. I am not familiar with the control interface for a modelcraft gear motor. You will need to look at the modelcraft electrical interface and see if it is compatible with the Zynq device I/O. The data sheet for the Zynq 7020 device found on the ZedBoard is available here: http://www.xilinx.com/support/documentation/data_sheets/ds187-XC7Z010-XC7Z020-Data-Sheet.pdf

     

    If you are using the PMOD interfaces on the ZedBoard the Zynq IO should be set to LVCMOS33. If you are using the LPC interface it can be set to 3.3V, 2.5V, or a 1.8V interface.

     

    -Gary