Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design AXI GPIO max rate?
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 4 replies
  • Subscribers 360 subscribers
  • Views 1350 views
  • Users 0 members are here
Related

AXI GPIO max rate?

e14 Contributor
e14 Contributor over 12 years ago

Hello,

I use one GP AXI Master Port to extend IO by adding AXI Interconnect IP and AXI GPIO IP. I test AXI GPIO rate, only 2MHz-3MHz.
In SDK, using code below
while(1)
{
  XGpio_DiscreteWrite(&LED_Ptr, 1, 0xffffffff);
  XGpio_DiscreteWrite(&LED_Ptr, 1, 0x00000000);
}
When I set FCLK_CLK0 100MHZ, GPIO rate is about 2.3MHz.If FCLK_CLK0 200MHZ, GPIO rate is about 3.6MHz.
I think it is too slow. What is the max rate for AXI GPIO? How to config ZYNQ to max AXI GPIO rate? Thanks!

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    I don't think the AXI GPIO function is ever going to be very high performance but you might try a more basic XGpio_WriteReg, which is a macro called by the XGpio_DiscreteWrite function, to strip out any time used by the function call (and the 'Xil_Assert' calls if any). Take a look at the XGpio_DiscreteWrite function:

     

     

    void XGpio_DiscreteWrite(XGpio * InstancePtr, unsigned Channel, u32 Data)

    {

                    Xil_AssertVoid(InstancePtr != NULL);

                    Xil_AssertVoid(InstancePtr->IsReady == XIL_COMPONENT_IS_READY);

                    Xil_AssertVoid((Channel == 1) ||

                                         ((Channel == 2) && (InstancePtr->IsDual == TRUE)));

     

                    XGpio_WriteReg(InstancePtr->BaseAddress,

                                                    ((Channel - 1) * XGPIO_CHAN_OFFSET) + XGPIO_DATA_OFFSET,

                                                    Data);

    }

     

    If you do try this let us know if it does improve the rate for you.

     

    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    I don't think the AXI GPIO function is ever going to be very high performance but you might try a more basic XGpio_WriteReg, which is a macro called by the XGpio_DiscreteWrite function, to strip out any time used by the function call (and the 'Xil_Assert' calls if any). Take a look at the XGpio_DiscreteWrite function:

     

     

    void XGpio_DiscreteWrite(XGpio * InstancePtr, unsigned Channel, u32 Data)

    {

                    Xil_AssertVoid(InstancePtr != NULL);

                    Xil_AssertVoid(InstancePtr->IsReady == XIL_COMPONENT_IS_READY);

                    Xil_AssertVoid((Channel == 1) ||

                                         ((Channel == 2) && (InstancePtr->IsDual == TRUE)));

     

                    XGpio_WriteReg(InstancePtr->BaseAddress,

                                                    ((Channel - 1) * XGPIO_CHAN_OFFSET) + XGPIO_DATA_OFFSET,

                                                    Data);

    }

     

    If you do try this let us know if it does improve the rate for you.

     

    -Gary