Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design AXI GPIO max rate?
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 4 replies
  • Subscribers 360 subscribers
  • Views 1352 views
  • Users 0 members are here
Related

AXI GPIO max rate?

e14 Contributor
e14 Contributor over 12 years ago

Hello,

I use one GP AXI Master Port to extend IO by adding AXI Interconnect IP and AXI GPIO IP. I test AXI GPIO rate, only 2MHz-3MHz.
In SDK, using code below
while(1)
{
  XGpio_DiscreteWrite(&LED_Ptr, 1, 0xffffffff);
  XGpio_DiscreteWrite(&LED_Ptr, 1, 0x00000000);
}
When I set FCLK_CLK0 100MHZ, GPIO rate is about 2.3MHz.If FCLK_CLK0 200MHZ, GPIO rate is about 3.6MHz.
I think it is too slow. What is the max rate for AXI GPIO? How to config ZYNQ to max AXI GPIO rate? Thanks!

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Hi all, good suggestion using XGpio_WriteReg.

    I am currently experimenting with the XGPio in Vivado. It seems the AXI GPIO block is software-driven, which is OK but I was more looking to control LEDs straight from other peripherals, like switches or buttons.
    Kind of a stepping stone before I get into looking at controlling the FMC.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Hi all, good suggestion using XGpio_WriteReg.

    I am currently experimenting with the XGPio in Vivado. It seems the AXI GPIO block is software-driven, which is OK but I was more looking to control LEDs straight from other peripherals, like switches or buttons.
    Kind of a stepping stone before I get into looking at controlling the FMC.