Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design AXI GPIO max rate?
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 4 replies
  • Subscribers 360 subscribers
  • Views 1353 views
  • Users 0 members are here
Related

AXI GPIO max rate?

e14 Contributor
e14 Contributor over 12 years ago

Hello,

I use one GP AXI Master Port to extend IO by adding AXI Interconnect IP and AXI GPIO IP. I test AXI GPIO rate, only 2MHz-3MHz.
In SDK, using code below
while(1)
{
  XGpio_DiscreteWrite(&LED_Ptr, 1, 0xffffffff);
  XGpio_DiscreteWrite(&LED_Ptr, 1, 0x00000000);
}
When I set FCLK_CLK0 100MHZ, GPIO rate is about 2.3MHz.If FCLK_CLK0 200MHZ, GPIO rate is about 3.6MHz.
I think it is too slow. What is the max rate for AXI GPIO? How to config ZYNQ to max AXI GPIO rate? Thanks!

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Another way to generate high frequency PWM or very short pulses is to use AXI Timer IP.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Another way to generate high frequency PWM or very short pulses is to use AXI Timer IP.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to e14 Contributor

    How can we use axi timer pwm and route this pwm signal to a pmod pin? Thank you.