Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design uenv.txt for embedded Linux
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 0 replies
  • Subscribers 358 subscribers
  • Views 259 views
  • Users 0 members are here
Related

uenv.txt for embedded Linux

100aditya
100aditya over 9 years ago

Dear Sir,

               A basic part of following question that i am going to ask i have already  asked on Microzed  hardware design and also i got the answer but still i am looking for some more answer as i have to do the same thing for mine ZedBoard Development. Here i am writing the content of uenv.txt file for U-boot:-

Line1-boot_microZed=mmcinfo;fatload mmc 0 Line2-0x3000000 2-${kernel_image}; fatload mmc 0 Line3-0x2FF0000 ${devicetree_image}; fatload mmc 0 Line4-0x2000000 ${ramdisk_image}; bootm Line5-0x3000000 0x2000000 0x2FF0000
Line6-uenvcmd   = run boot_microZed
Line7-uenv_boot = run boot_microZed

So here are mine questions:-

1- In Above uenv.txt  "boot_microZed" is simply a variable and for example i can replace  it(let us say for mine ZedBoard), with "boot_Zedboard". So if i do this then i have to replace "boot_microZed" with "boot_Zedboard" at all the places only in this uenv.txt file, not anywhere else. I want to say that boot_microZed is not a board specific command and it is just simply a variable. If i am not correct please correct me.

2- I do not get why at line 6 and line 7 the command "run boot_microZed" is being called two times in two different variables i.e unvcmd and uenv_boot.

3- what are this unvcmd and uenv_boot  variables ? are they board specific? If it is from where i can get the information about it.

Please answer me ????

Regards

Aditya