Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design Write Data to Sdcard of Zedboard
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 8 replies
  • Subscribers 360 subscribers
  • Views 1518 views
  • Users 0 members are here
Related

Write Data to Sdcard of Zedboard

e14 Contributor
e14 Contributor over 10 years ago

Hi folks,
I want to write data/file to Sdcard present in Zedboard. I am able to write data to DRAM. How Can i Read from DRAM and write that particular data to SDCARD?
I have searched but not able to find any good tutorial for this.

Regards

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    You don't have to do the complete lab of data logging using  the OLED screen. Just create a Zynq Processing System ,do procedure B (Enable SD0 Host Controller on PS ) exactly as explained in the tutorial(cuz the default settings of Vivado r wrong). Then procedure C and D. However, in procedure E you need to create your own application. Read the FatFs API sections to be able to use it.
    http://embeddedcentric.com/data-logging-using-sd-cards/

    Hope this helps.

    EmbeddedCentric.com

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to e14 Contributor

    I have another question. I want to write minimum 256 MB or more to DDR memory of Zed Board. Total size of DDR is 512 MB. And then want to read all the data which i have wrote in memory. I am able to write 64 bytes of data in DDR but not able to write more than that. To write in DDR I am using Axi_dma on PL side.

    And one more question i want to ask do i have to enable the READ CHANNEL of Axi_dma to read from DDR???

    I have posted a new forum here (http://zedboard.org/content/read-and-write-ddr-zed-board) but no one answered So Please help Sir.

    Regards

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to e14 Contributor

    I have another question. I want to write minimum 256 MB or more to DDR memory of Zed Board. Total size of DDR is 512 MB. And then want to read all the data which i have wrote in memory. I am able to write 64 bytes of data in DDR but not able to write more than that. To write in DDR I am using Axi_dma on PL side.

    And one more question i want to ask do i have to enable the READ CHANNEL of Axi_dma to read from DDR???

    I have posted a new forum here (http://zedboard.org/content/read-and-write-ddr-zed-board) but no one answered So Please help Sir.

    Regards