Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design Fixed interval timer interrupt example?
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 5 replies
  • Subscribers 362 subscribers
  • Views 1390 views
  • Users 0 members are here
Related

Fixed interval timer interrupt example?

jesusmgonzalez
jesusmgonzalez over 12 years ago


Hi,

I'm trying to develop a small example using this IP through interrupts. I saw some examples using Timers,
but I would like to use this IP.

Does someone know where could I get some kind of information?

Thanks,

  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Once you have exported your hardware design to SDK open up the system.mss file (under the 'bsp folder in the Project Explorer pane on the left) and click on the 'examples' link to the right of the timer you want to use in the 'Peripheral Drivers' section. The interrupt drive example code should give you a good start.

     

    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jesusmgonzalez
    0 jesusmgonzalez over 11 years ago

    Hi,
    Thanks for the answer, but for this IP there is no example code exported from hardware designs, or I can't find it.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    I would suggest using the 'interrupt' version of the example code for one of the timer IP that is supplied as a starting point. Just strip out the portion of the code that initializes and re-programmes the timer.

     

    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • k@hh
    0 k@hh over 9 years ago

    @TroutChaser I think you've understood @jesusmgonzalez wrong. He want to use the "Fixed Interval Timer" this Timer has no AXI connection and therefore no drivers. I have the same problem here could run the Interrupt example with the AXI Timer but not with some non AXI IP core. I've been looking for quite a while but can't find an answer. I've defined the Port as Interrupt Port and connected it via concat to the IRQ of the Zynq. It schows up with a number in my xparameters.h file but the initialization via XScuGic_Connect, XScuGic_SetPriorityTriggerType and XScuGic_Enable will trigger nothing. The GIC initialisation is done the same way as at the AXI Timer example. The only thing that is not clear is the last parameter of the XScuGic_Connect function (I've tried 0 and &InterruptController (from XScuGic_CfgInitialize)). So does someone no how to do that?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • k@hh
    0 k@hh over 9 years ago

    https://forums.xilinx.com/t5/Embedded-Development-Tools/HOW-TO-SETUP-AN-INTERRUPT-FOR-AN-AXI-GPIO-WHICH-OCCURS-AT-RISING/td-p/312737

    I've found a Solution I was just copying the code from stephenm (05-15-2013 03:56AM) and it worked... Put my Code in the same initialisation direction as in his code and it worked as well... very weird. I Just throw out the second Interrupt and replaced the Interrupt Number with my define from my xparameters.h file.