Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design Using ethernet with Microblaze
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 9 replies
  • Subscribers 359 subscribers
  • Views 1963 views
  • Users 0 members are here
Related

Using ethernet with Microblaze

Former Member
Former Member over 10 years ago

Hi,
I want to use Ethernet to connect my Microblaze based design to my PC. Is it possible without using Zynq processor. How can this be accomplished?

  • Sign in to reply
  • Cancel
Parents
  • Former Member
    0 Former Member over 10 years ago

    No.

     

    If you take a look at the block diagrams in the Zynq Technical Reference Manual ( http://www.xilinx.com/support/documentation/user_guides/ug585-Zynq-7000-TRM.pdf ) you will see that the MIO connections you can access via the EMIO are the 'device' side of the connection, not the 'user interface' side. That is you could connect the GMII/RGMII connection from one of the PS Ethernet MACs via EMIO but there is no way to access the registers that control the Ethernet MAC or those that transfer the data. Same with the SD Card. You could make a connection to an external SD Card but would not be able to control the SD Card controller or transfer data via the EMIO connection.

     

    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Former Member
    0 Former Member over 10 years ago

    No.

     

    If you take a look at the block diagrams in the Zynq Technical Reference Manual ( http://www.xilinx.com/support/documentation/user_guides/ug585-Zynq-7000-TRM.pdf ) you will see that the MIO connections you can access via the EMIO are the 'device' side of the connection, not the 'user interface' side. That is you could connect the GMII/RGMII connection from one of the PS Ethernet MACs via EMIO but there is no way to access the registers that control the Ethernet MAC or those that transfer the data. Same with the SD Card. You could make a connection to an external SD Card but would not be able to control the SD Card controller or transfer data via the EMIO connection.

     

    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
No Data