Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design Zedboard 512x512 matrices, % utilization problem
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 361 subscribers
  • Views 931 views
  • Users 0 members are here
Related

Zedboard 512x512 matrices, % utilization problem

jmales
jmales over 11 years ago

My objective is to read seven 512X512 float matrices from the SD card to the DDR memory (step accomplished already with each matrix occupying around 1Mb), then pass them from DDR to my custom IP block (I'm doing this transition with AXI DMA block), normalize them innside the custom IP block and then output them to DDR memory (also with the AXI DMA block).

Well, I'm doing my custom IP block in Vivado HLS and following the steps that I saw in this Xilinx manual (which shall be the ideal way to do this since its from Xilinx): http://www.xilinx.com/support/documentation/application_notes/xapp1170-zynq-hls.pdf

It works for a 32x32 matrix.

But unfortunately, when increasing the matrix dimensions to 512x512, even doing only a multiplication by 2.0 of each matrix' parameter, the BRAM_18K utilization is 365%!!

What can I do do brutaly decrease the % of resources used? I'll need to do lots of operations to the matrices inside the custom IP block and if a simple multiplication by 2.0 uses 365% of BRAMs a solution that decreases the amount of this example to 80/90% is not good enough. What I'm looking for is a solution that sets the BRAM utilization to around 5% in this example.

  • Sign in to reply
  • Cancel
Parents
  • Former Member
    0 Former Member over 11 years ago

    This question is Xilinx tool related and is probably better targeted to one of the Xilinx Community forums, perhaps the HLS forum in particular: http://forums.xilinx.com/t5/High-Level-Synthesis-HLS/bd-p/hls

     

    That said, as I am sure you know, multiplying 512 x 512 float is a pretty hefty operation and you just may need to target a Zynq device with more BRAM than the 7020 device on the ZedBoard. You might want to look at a PicoZed 7030 or the one of the Zynq MMP or Mini-ITX boards with a 7045 or 70100 device.

     

    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Former Member
    0 Former Member over 11 years ago

    This question is Xilinx tool related and is probably better targeted to one of the Xilinx Community forums, perhaps the HLS forum in particular: http://forums.xilinx.com/t5/High-Level-Synthesis-HLS/bd-p/hls

     

    That said, as I am sure you know, multiplying 512 x 512 float is a pretty hefty operation and you just may need to target a Zynq device with more BRAM than the 7020 device on the ZedBoard. You might want to look at a PicoZed 7030 or the one of the Zynq MMP or Mini-ITX boards with a 7045 or 70100 device.

     

    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • jmales
    0 jmales over 11 years ago in reply to Former Member

    I also tried posting there but that community is really slow and no one answers...

    So do you mean that I can't even multiply 512x512 matrices in a Zedboard in your opinion? So what's the FPGA side of the Zedboard for? I see no use for it if it can't even do a simple operation (in the software world as you know, 512x512 matrices' operations are considered very very simple ones)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer