Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design Read SD Card from PS Part
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 359 subscribers
  • Views 484 views
  • Users 0 members are here
Related

Read SD Card from PS Part

e14 Contributor
e14 Contributor over 11 years ago

Hi

I am trying to implement a System on Zedboard and I need to read files from SD card from PS part and use that data.

I searched a lot about this implementation and I came up with using AXI SPI Interface and use it for making this connection. But, I couldn't find anything about the rest of the implementation. Can anyone help me what to do or introduce any tutorial or link that could help me to connect SD Card to PS?

I'm in hurry, So, Please help me.

Thanks

  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    The SD Card on the Zedboard is directly connected to the PS SD 0 controller. You do not say if your application is 'bare metal' or using an operating system such as Linux.

     

    Assuming bare metal you can open the system.mss file in the SDK, once you have generated a BSP, and click on the 'Documentation' link to the right of the 'ps7_sd_0' in the Peripheral Drivers section for code examples.

     

    You could also generate an FSBL for you design and take a look at the code included for SD Card access there.

     

    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to e14 Contributor

    Hi TroutChaser,

    Thanks for your help. I used SD0 and XPS generated NetList perfectly. Then, I tried to use FSBL and I made an FSBL application project, but when I use SDCard code, there is a problem with InitSD() function. Please look at this code:

    Status = InitSD("test.txt");
    if (Status != XST_SUCCESS) {
    tfsbl_printf(DEBUG_GENERAL,"SD_INIT_FAILr
    ");
    tOutputStatus(SD_INIT_FAIL);
    tFsblFallback();
    t}
    MoveImage = SDAccess;
    fsbl_printf(DEBUG_INFO,"SD Init Done r
    ");

    when this code ran, InitSD() return XST_FAILURE and it seems that it cannot initialize "test.txt" file. I copied "test.txt" file in SDCard ,already.

    The InitSD function is here:

    u32 InitSD(const char *filename)
    {

    tFRESULT rc;

    t/* Register volume work area, initialize device */
    trc = f_mount(0, &fatfs);
    tfsbl_printf(DEBUG_INFO,"SD: rc= %.8x
    r", rc);

    tif (rc != FR_OK) {
    ttreturn XST_FAILURE;
    t}

    tstrcpy_rom(buffer, filename);
    tboot_file = (char *)buffer;
    tFlashReadBaseAddress = XPAR_PS7_SD_0_S_AXI_BASEADDR;

    trc = f_open(&fil, boot_file, FA_READ);
    tif (rc) {
    ttfsbl_printf(DEBUG_GENERAL,"SD: Unable to open file %s: %d
    ", boot_file, rc);
    ttreturn XST_FAILURE;
    t}

    treturn XST_SUCCESS;

    }

    Can you help me with this error, Please?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    There are a couple of previous forum threads that might be useful:

     

    http://zedboard.org/content/standalone-sd-card-sdio

    http://zedboard.org/content/sd-card-example-design-using-standalone

     

    You should make sure that you have a good SD Card that has been formatted correctly and works with the ZedBoard. You might want to load a known good boot file on it and verify the card is good.

     

    -Gary