Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design SPI Interface
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 3 replies
  • Subscribers 359 subscribers
  • Views 502 views
  • Users 0 members are here
Related

SPI Interface

Former Member
Former Member over 10 years ago

Hi,
I have a design in which Microblaze read data at its interface and saves data on the Flash Memory (Spansion S25FL256S) available on Zedboard by using Xilinx Quad SPI Core. If some body could help me that at which pins I should connect the SPI Core output pins so that I should be able to connect to the SPI Flash available on board.
Regards

  • Sign in to reply
  • Cancel
Parents
  • Former Member
    0 Former Member over 10 years ago

    Hello Habib,

     

    The QSPI Flash Memory on the ZedBoard is directly connected to Zynq MIO type pins, which can only be driven from the Zynq PS (Processing System). The only way to control this Flash Memory is by using the Zynq PS SPI controller, it is not available to a Quad SPI Core in the Zynq PL (Programmable Logic) section.

     

    You could add an SPI Flash Memory to one of the PL PMOD connectors on the ZedBoard and drive it directly from the PL. Something like this PMOD: http://store.digilentinc.com/pmodsf2-serial-pcm-128-mbit/

     

    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Former Member
    0 Former Member over 10 years ago

    Hello Habib,

     

    The QSPI Flash Memory on the ZedBoard is directly connected to Zynq MIO type pins, which can only be driven from the Zynq PS (Processing System). The only way to control this Flash Memory is by using the Zynq PS SPI controller, it is not available to a Quad SPI Core in the Zynq PL (Programmable Logic) section.

     

    You could add an SPI Flash Memory to one of the PL PMOD connectors on the ZedBoard and drive it directly from the PL. Something like this PMOD: http://store.digilentinc.com/pmodsf2-serial-pcm-128-mbit/

     

    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
No Data