Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design Cannot use SD Card partition as root filesystem
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 5 replies
  • Subscribers 360 subscribers
  • Views 1630 views
  • Users 0 members are here
Related

Cannot use SD Card partition as root filesystem

e14 Contributor
e14 Contributor over 11 years ago

I am desperately trying to boot the last Xilinx Linux kernel on my rev. D ZedBoard with the root file system on the SD Card. Apparently there is a hardware problem:

mmc0: new high speed SDHC card at address 0007
mmcblk0: mmc0:0007 SD04G 3.70 GiB (ro)
mmcblk0: p1 p2
VFS: Cannot open root device "mmcblk0p2" or unknown-block(179,2): error -30
Please append a correct "root=" boot option; here are the available partitions:
b300         3887104 mmcblk0  driver: mmcblk
  b301          204800 mmcblk0p1 be93329c-01
  b302         3681280 mmcblk0p2 be93329c-02
Kernel panic - not syncing: VFS: Unable to mount root fs on unknown-block(179,2)

As can be seen in the log, the mmcblk0p2 partition is proposed as a valid available partition but the kernel could not open it... My bootargs (in device tree) specifies the rootwait option:

bootargs = "console=ttyPS0,115200 root=/dev/mmcblk0p2 rw rootwait earlyprintk";

but it seems to have no effect. Is there something wrong with the &sdhci0 entry of my device tree? I tried:

&sdhci0 {
tclock-frequency = <50000000>;
tstatus = "okay";
};

and:

&sdhci0 {
tstatus = "okay";
};

None worked. I tried with two other ZedBoards rev. C and... it worked. Is there something wrong with the rev. D?

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    Anyone have more updates on this?  I also am seeing the (ro) issue on boot with the latest 4.4 kernel ...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to e14 Contributor

    Aaaaand as soon as I posted this I saw that I had the xlconstant block set to 1 rather than 0 for the WP input on the PS7 on my BD ... so there that is.

    Hope fully that helps someone else.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to e14 Contributor

    Aaaaand as soon as I posted this I saw that I had the xlconstant block set to 1 rather than 0 for the WP input on the PS7 on my BD ... so there that is.

    Hope fully that helps someone else.