Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design A problem with the HDMI on the zedboard in vivado 2014.3
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 1 reply
  • Subscribers 359 subscribers
  • Views 213 views
  • Users 0 members are here
Related

A problem with the HDMI on the zedboard in vivado 2014.3

e14 Contributor
e14 Contributor over 11 years ago

Hi,



I'm trying to creat a running hdmi output on the zedbord in vivado 2014.3.

Altough the same tcl scripts run smoothly in 2014.2, now I have the following error message:



ERROR: [IP_Flow 19-3461] Value 'IIC_MAIN' is out of the range for parameter 'IIC Board Interface(IIC_BOARD_INTERFACE)' for BD Cell '/axi_iic_main' . Valid values are - Custom



I tried to add manually add an IIC ip to a block design, and looked for its IIC_BOARD_INTERFACE, and it was "Custom", so I tried to modify the in .tcl file rewriting the axi_iic_main to Custom, but then I get:



can't read "custom": no such variable



I totally don't understand, what can be wrong or why can it be wrong?



Best,

Deni

  • Sign in to reply
  • Cancel
  • henry10210
    0 henry10210 over 11 years ago

    If you change {IIC_MAIN} to IIC_MAIN, you can get past this particular problem, but then you will see this soon thereafter; I am reinstalling Vivado 2014.2 right now.

    WARNING: command 'get_bus_interface' will be removed in the 2014.3 release, use 'get_bus_interfaces' instead
    ERROR: [Common 17-39] 'set_property' failed due to earlier errors.

        while executing
    "set_property ENABLEMENT_DEPENDENCY $dependency $port"
        ("foreach" body line 2)
        invoked from within
    "foreach port [ipx::get_ports [format "%s%s" $port_prefix "*"]] {
    ttset_property ENABLEMENT_DEPENDENCY $dependency $port
    t}"
        (procedure "adi_set_ports_dependency" line 2)
        invoked from within
    "adi_set_ports_dependency $prefix $dependency"
        (procedure "adi_set_bus_dependency" line 3)
        invoked from within
    "adi_set_bus_dependency "M_AXIS" "M_AXIS"
    t"(spirit:decode(id('MODELPARAM_VALUE.C_DMA_TYPE')) = 0)""
        (file "./axi_i2s_adi_ip.tcl" line 60)
    update_compile_order -fileset sim_1