Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design OLed within own Planahead Linux Project
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 359 subscribers
  • Views 390 views
  • Users 0 members are here
Related

OLed within own Planahead Linux Project

eactor
eactor over 12 years ago

Hello,
I successfully used the zed_oled device under /dev/ with the original SD Card that came with the board. Therefore I used the post from ZynqGeek (http://www.zedboard.org/content/zedboard-oled) and the Octave/Matlab script from the first reply.

Now I wanted to add the OLED ability to my own Planahead/Linux project. Therefore I added the PMOD driver to the kernel (menuconfig -> devices-> PMOD -> PMODOLED) and included the following into the devicetree (Kernel documentation pmodoled.txt) :

zed_oled {
compatible = "dglnt,pmodoled-gpio";
/* GPIO Pins */
vbat-gpio = <&gpio 55 0>;
vdd-gpio = <&gpio 56 0>;
res-gpio = <&gpio 57 0>;
dc-gpio = <&gpio 58 0>;
/* SPI-GPIOs */
spi-bus-num = <2>;
spi-sclk-gpio = <&gpio 59 0>;
spi-sdin-gpio = <&gpio 60 0>;
};

Thereby gpio referece to:

gpio: gpio@e000a000 {
tcompatible = "xlnx,ps7-gpio-1.00.a";
treg = <0xe000a000 0x1000>;
tinterrupts = <0 20 0>;
tinterrupt-parent = <&gic>;
tgpio-controller;
t#gpio-cells = <2>;
};

At this point I ask myself is a real hardware SPI0 or SPI1 of the PS connected to those pins, since it seems to be an SPI connection towards the OLED and do I have to configure that within Planahead. Or in the other case is the SPI imitated by the Linux driver? I also had a look into the schematic and constrain file to make sure the Signals are connected to the right pins:
NET OLED_DC       LOC = U10  | IOSTANDARD=LVCMOS33;  # "OLED-DC"
NET OLED_RES      LOC = U9   | IOSTANDARD=LVCMOS33;  # "OLED-RES"
NET OLED_SCLK     LOC = AB12 | IOSTANDARD=LVCMOS33;  # "OLED-SCLK"
NET OLED_SDIN     LOC = AA12 | IOSTANDARD=LVCMOS33;  # "OLED-SDIN"
NET OLED_VBAT     LOC = U11  | IOSTANDARD=LVCMOS33;  # "OLED-VBAT"
NET OLED_VDD      LOC = U12  | IOSTANDARD=LVCMOS33;  # "OLED-VDD"

Still Iu2019m stuck since no device entry is created within the dev folder and no entry of the oled can be seen within /proc/device-tree/amba@0/... Or /proc/iomem/. There an SPI e000d000 is stated even if not declared within the devicetree, but unsure if it is related to the OLED.
Thanks for help
eactor

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 9 years ago

    I never liked to write anything. Code writing is more about me. Recently, I have been asked to write a program on Education.

    I use Linux when I pay for essay for my IT projects.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 9 years ago

    I never liked to write anything. Code writing is more about me. Recently, I have been asked to write a program on Education.

    I use Linux when I pay for essay for my IT projects.