Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design Setting up PLL for use with FPGA fabric
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 3 replies
  • Subscribers 357 subscribers
  • Views 728 views
  • Users 0 members are here
  • pll
Related

Setting up PLL for use with FPGA fabric

hawx2020
hawx2020 over 1 year ago

Hi,

I'm having trouble setting up the 33MHz PLL clock so that I am able to access it from the FPGA fabric. I've never used a PLL before and I've only ever used the FPGA fabric on the zedboard so I'm not quite sure where to start. If anyone has any advice or an example project, that would be greatly appreciated.

Thanks!

  • Sign in to reply
  • Cancel
  • iksevas
    iksevas over 1 year ago

    Stupid question but what platform are you targeting? Most of the SOC (Zynq-7000) or MPSoC (Zynq UltraScale) have a 33MHz reference clock into the system - there is a simple GUI in Vivado that will allow you to forward a version of this clock to the FPGA fabric for use. This clock can be synthesized into different frequencies depending on your need. It should be as simple as setting up your block design properly in the tools.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • hawx2020
    hawx2020 over 1 year ago in reply to iksevas

    Hi, it's the Zynq-7000 XC7Z020-CLG484-1. I tried following some tutorial that was using the block designs, but I couldn't get it to work. I was probably doing something wrong though. Do you have an example?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • iksevas
    iksevas over 1 year ago in reply to hawx2020

    The PicoZed product targets that device. There are reference designs on this page:

    https://www.avnet.com/wps/portal/us/products/avnet-boards/avnet-board-families/picozed/

    More up-to-date BSPs are on a SHAREPOINT site. https://avnet.me/ZedSupport

    Either way, you will see in the Vivado portions that there is typically a 100MHz fabric clock provided from the block design that gets created from the 33MHz reference clock.