Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design Connecting Zedboard to Vivado - Hardware Manager not Detecting
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 4 replies
  • Subscribers 357 subscribers
  • Views 1060 views
  • Users 0 members are here
Related

Connecting Zedboard to Vivado - Hardware Manager not Detecting

eb_air
eb_air over 1 year ago

Hello,

I have been struggling to detect my Zedboard on Vivado's Hardware Manager run in a Linux OS. When I went into the Hardware Manager, I could connect into the local hardware server, but the Zedboard did not show up. I used version 2023.2 and 2022.2, but both versions had the same problem. I tried the JTAG and UART modes with no success. I am confused with the problem here because if I run lsusb, I see "232H Single HS USB-UART/FIFO IC" for the JTAG interface and "Cypress Semiconductor Corp. CDC ACM serial port", which I assume means the drivers are properly installed.

Is there something I am doing wrong here?

  • Sign in to reply
  • Cancel
  • dyessgg
    0 dyessgg over 1 year ago

    Did you load the JTAG cable drivers?  They don't install as part of Vivado installation.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • eb_air
    0 eb_air over 1 year ago in reply to dyessgg

    I have not done that yet. Is that in "data/xicom/cable_drivers/lin64/install_script/install_driver" ? If not, where can I find it?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • dyessgg
    0 dyessgg over 1 year ago in reply to eb_air

    If I remember correctly, that is the location of the script.  It's actually just setting up some udev rules for the USB device.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • eb_air
    0 eb_air over 1 year ago in reply to dyessgg

    Alright, I will look into that.