Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design Build me an Embedded Processing System and I'll Give You a Zynq®︎-7000 SoC ZC702 Evaluation Kit
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 26 replies
  • Subscribers 371 subscribers
  • Views 5297 views
  • Users 0 members are here
  • fpga_featured
  • scasny
  • xilinx
  • avnet_featured
  • scasny_web
Related

Build me an Embedded Processing System and I'll Give You a Zynq®︎-7000 SoC ZC702 Evaluation Kit

rscasny
rscasny over 7 years ago

I was in the right place at the right time. I was asked, "I have two ZynqRegistered-7000 SoC ZC702 Evaluation Kits, would you like them?" For one second I paused, and declared," YES!"

image

So, here I am, sitting at my desk in the element14 offices in Chicago with two fairly big boxes to giveaway to the right people. Don't know much about the ZynqRegistered-7000 SoC ZC702 Evaluation Kit? Let me fill you in a bit: It has all components of hardware, design tools, IP, and pre-verified reference designs to enable you to build a complete embedded processing platform. It includes pre-verified reference designs and industry-standard FPGA Mezzanine Connectors (FMC) allow scaling and customization with daughter cards. A picture is worth a thousand, so here's a short video for you to take a look-

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

Here's the features and benefitsfeatures and benefits:

 

  • Optimized for quickly prototyping embedded applications using Zynq-7000 SoCs
  • Hardware, design tools, IP, and pre-verified reference designs
  • Demonstrates a embedded design, targeting video pipeline
  • Advanced memory interface with 1GB DDR3 Component Memory
  • Enabling serial connectivity with USB OTG, UART, IIC, CAN Bus
  • Supports embedded processing with Dual ARM Cortex-A9 core processors
  • Develop networking applications with 10-100-1000 Mbps Ethernet (GMII, RGMII and SGMII)
  • Implement Video display applications with HDMI out
  • Expand I/O with the FPGA Mezzanine Card (FMC) interface

 

How to Get One of These Kits?

 

I'd like to get some ideas or proposals for an embedded project that uses these kits. Consider the proposals like a Design challenge for Programmable Devices -- something we haven't done yet. What would you build or Prototype? Tell me the how's and why's of it. I don't expect you to change the world, but I'd like to use these kits for a project with a WoW factor. Please enter your project idea in the comment section below.

 

Sincerely,

 

Randall Scasny

RoadTest Program Manager

  • Sign in to reply
  • Cancel

Top Replies

  • 14rhb
    14rhb over 7 years ago +6
    That is a very capable board with a great range of FMC addon boards. As a stand alone system (albeit perhaps with addition of a low-cost PMod card) I would like to see the following built: Logic and Protocol…
  • Attila Tőkés
    Attila Tőkés over 7 years ago +5
    Although is not from the latest generation, the Xilinx Zynq-7000 SoCs is still really powerful and can be used for compute intensive applications. I tough to create a (series of) tutorial (s) on: Hardware…
  • avnrdf
    avnrdf over 7 years ago +4
    How about a wideband (multi-channel) spectrum analyzer? Analog Devices makes SDR boards and even supplies an image for the ZC702 (decimator + interface logic in the FPGA, and Linux + other software on…
Parents
  • Attila Tőkés
    Attila Tőkés over 7 years ago

    Although is not from the latest generation, the Xilinx Zynq-7000 SoCs is still really powerful and can be used for compute intensive applications.

     

    I tough to create a (series of) tutorial(s) on:

    Hardware Accelerated Image Processing and Machine Learning using Xilinx SDSoCTm

     

    SDSoCTm is Xilinx's Software Defined Development platform. It allows targeting FPGA-s without too much hardware knowledge. For example you can easily create hardware (PL/FPGA) accelerated versions C/C++ functions.

     

    Xilinx reVision is a set of hardware accelerated libraries for computer vision (xfOpencv) and machine learning (Caffe).

     

    I want to create some examples for the ZynqRegistered-7000 SoC ZC702 Evaluation Kit to demonstrate hardware accelerated:

    • image processing algorithms (xfOpenCV) - 2D filters, edge / object detection, etc.
    • machine learning algorithms (Caffe) - binary neural networks

     

    Hardware:

    ZynqRegistered-7000 SoC ZC702 Evaluation Kit

    USB Webcam - Logitech C920

    HDMI Monitor

     

    Software:

    Vivado Design Suite - hardware design

    Xilinx SDK IDE - embedded development

    Xilinx SDx IDE - software defined development

    Xilinx reVision (xfOpencv, Caffe) - hardware accelerated image processing and BNN-s

    PetaLinux - Xilinx's Linux Distribution for FPGA based SoC-s

     

    Check out my Stereo Vision and LiDAR Powered Donkey Car project which uses the Xilinx Zynq UltraScale+ MPSoC ZU3EG SBVA484 for hardware accelerated stereo vision.

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Cancel
  • rscasny
    rscasny over 7 years ago in reply to Attila Tőkés

    I agree that's not probably not the latest generation. I was given the two kits by a representative of Xilinx. I took them because I wanted to give some of our members a chance to work with the kit.

     

    Randall

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • rscasny
    rscasny over 7 years ago in reply to Attila Tőkés

    I agree that's not probably not the latest generation. I was given the two kits by a representative of Xilinx. I took them because I wanted to give some of our members a chance to work with the kit.

     

    Randall

    • Cancel
    • Vote Up +4 Vote Down