Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZUBoard fingerprit error when I'm testing the AES-ACC-DUALCAM-G module on ZUBoard1CG
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 1 reply
  • Answers 1 answer
  • Subscribers 363 subscribers
  • Views 765 views
  • Users 0 members are here
Related

fingerprit error when I'm testing the AES-ACC-DUALCAM-G module on ZUBoard1CG

wolfa
wolfa over 3 years ago

The failure happens when using pre-built SD card Image (2021.2) by using following command: python3 avnet_dualcam_ar0144_stereo_face_detection.py . It seems that  there is an architecture mismatch between the DPU in the platform and the compiled XMODEL. Is there any newer version of pre-built SD card image available that i can use for demonstration purposes. when not I'm need to dive deeper according Xilinx answer record: support.xilinx.com/.../DPU-fingerprint-ERROR Thanks Andreas

  • Sign in to reply
  • Cancel
  • wolfa
    0 wolfa over 3 years ago

    Thanks Mario for your clarification. The compiled models for B128 DPU are already build and the Dual-Cam demo runs by change the symbolic link.

    For the guys who are interested  attached the procedure as provided by Mario.

    Regards from Germany

    Andreas

    When you get the following error message:

    model_fingerprint 0x1000020f6012200 dpu_fingerprint 0x1000020e2012208

    It means that you are trying to use the B512 models with the B128 design (dualcam), which is invalid (and not possible).

     

     

    You need to change the following symbolic link to point to the correct models.  Here is an excerpt from the hackster project:

                   http://avnet.me/avnet-zub1cg-sbc-2021.2

     

    Before running the demos, we need to verify that we are using the B128 version of the pre-compiled ModelZoo, as shown below:

    $ cd /usr/share/vitis_ai_library/
    $ ls -la
    total 40
    drwxr-xr-x   6 root root  4096 Sep 16  2022 .
    drwxr-xr-x  84 root root  4096 Mar  9 12:34 ..
    lrwxrwxrwx   1 root root    11 Mar  9 12:34 models -> models.b512
    drwxr-xr-x 147 root root 12288 Sep 16  2022 models.b128
    drwxr-xr-x 223 root root 12288 Sep 16  2022 models.b512
    drwxr-xr-x   5 root root  4096 Mar  9 12:34 samples
    drwxr-xr-x  58 root root  4096 Mar  9 12:34 test

    $ rm models
    $ ln -sf models.b128 models
    $ ls -la
    total 40
    drwxr-xr-x   6 root root  4096 Mar  9 13:05 .
    drwxr-xr-x  84 root root  4096 Mar  9 12:34 ..
    lrwxrwxrwx   1 root root    11 Mar  9 13:05 models -> models.b128
    drwxr-xr-x 147 root root 12288 Sep 16  2022 models.b128
    drwxr-xr-x 223 root root 12288 Mar  9 13:05 models.b512
    drwxr-xr-x   5 root root  4096 Mar  9 12:34 samples
    drwxr-xr-x  58 root root  4096 Mar  9 12:34 test

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer