Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZUBoard How to use the MAC Address from EEPROM in U-Boot?
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 363 subscribers
  • Views 3300 views
  • Users 0 members are here
  • ZUBoard
Related

How to use the MAC Address from EEPROM in U-Boot?

Tim5000
Tim5000 over 3 years ago

Hi, has anyone had experience of getting U-Boot in Petalinux 2023.1 to read the MAC Address out of the AT24MAC602 EEPROM at startup and use it rather than the random one?

Warning: ethernet@ff0d0000 (eth0) using random MAC address - XX:XX:XX:XX:XX:XX

I've successfully been able to read the MAC Address and serial number out of the EEPROM's special area (device address mapped to 0x58) using debug commands in both U-Boot and Linux.

Reading 6 octets from device address 0x58, address 0x9a in Linux yields the MAC Address (Atmel OUI retained here for confirmation).

sudo i2ctransfer -y 0 w1@0x58 0x9a r6
0xfc 0xc2 0x3d 0xXX 0xXX 0xXX

U-Boot

ZynqMP> i2c dev 0
Setting bus to 0
ZynqMP> i2c md 0x58 0x9a 6
009a: fc c2 3d XX XX XX

I believe since 2022 U-Boot has removed some of the compile defines and how the EEPROM is used so I believe it needs something like this:

components/plnx_workspace/device-tree/device-tree/system-top.dts

/ {

aliases {

nvmem0 = &eeprom;

};

};

project-spec/meta-user/recipes-bsp/device-tree/files/system-user.dtsi

&i2c0 {
    eeprom: eeprom@58{
        compatible = "atmel,24c02";
        reg = <0x58>;
        read-only;
        pagesize = <16>;

        eth0_addr: eth-mac-addr@9A { /* 9A is the address in the EEPROM */
            reg = <0x9A 0x06>;
        };
    };
};

But U-Boot is still using the randomised address.

Any pointers would be helpful.

Thanks

  • Sign in to reply
  • Cancel
  • Tim5000
    0 Tim5000 over 3 years ago

    I've also found that if I set the mac address in petalinux-config (via Subsystem AUTO Hardware Settings) it will correctly take that instead of the randomised one, but obviously the goal here is to pull it from the actual EEPROM ideally.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Navin_08
    0 Navin_08 over 2 years ago

    Hi Tim5000 can you please share me the details where can I find the BSP for ZUBOARD 1CG , even I want to build an image in petalinux for my project usage.