Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZUBoard Compliant Power Supply for the ZU1CG board and First bootup in Linux
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 3 replies
  • Subscribers 365 subscribers
  • Views 1134 views
  • Users 0 members are here
  • zync
  • ZU1CG
Related

Compliant Power Supply for the ZU1CG board and First bootup in Linux

sapta15
sapta15 over 2 years ago

Hello Community! 
I am relatively a novice in the FPGA community and just started with the ZU1CG board. I have two queries 

(1)  I am using a Samsung EP-T4510 45 W, Power Delivery 3.0, Fast Charge adapter to power it and all the LEDs are running as demonstrated in getting started video. However, The board is getting extremely hot and I am worried that I am burning something. The board should be able to handle 45 W and the charger is PD compliment thus should negotiate with the board about the power requirements. Am I doing something wrong?

(2) About the first boot in a Ubuntu environment. Following the startup guide, I have booted up the board but do not see anything on the Serial port. Please note I am not even opening up the VITIS. There is supposed to be an RTOS installed there with a web interface to control the LEDs in the beginning. Do I have to burn the image with Petal Linux in an SD card and then boot up from it, to get a Serial port communication or I am doing something very wrong here? The getting started guide isn't really that helpful in the case of Linux users. 

  • Sign in to reply
  • Cancel

Top Replies

  • padudle
    padudle over 2 years ago +1 verified
    The high temperature is normal. Personally, I am glad it does not have a fan because the fan noise gets annoying very quickly. I don't remember what Avnet provides for getting started. If you desire…
  • andycap
    0 andycap over 2 years ago

    My one gets extremely hot as well, I think it is normal. I have a desk fan pointing at it.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • padudle
    +1 padudle over 2 years ago

    The high temperature is normal. Personally, I am glad it does not have a fan because the fan noise gets annoying very quickly.

    I don't remember what Avnet provides for getting started.  If you desire to run desktop linux on the board you could look at this github project, https://github.com/hdlguy/zuboard

    It contains an fpga design and instructions to use Petalinux to boot Debian on it.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • sapta15
    0 sapta15 over 2 years ago in reply to padudle

    Thanks a lot. Will try definitely to boot Debian!