Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZUBoard ZUBoard baremetal SD boot problem
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 13 replies
  • Answers 1 answer
  • Subscribers 362 subscribers
  • Views 2031 views
  • Users 0 members are here
  • baremetal
  • ZUBoard
  • boot
  • sd
Related

ZUBoard baremetal SD boot problem

tony56887
tony56887 over 1 year ago

I'm unable to boot a simple baremetal app from the SD card. Very strange problem.

  • The ZUB will boot petalinux from the SD card just fine, I've built and booted the ZUB petalinux base and trifecta builds. All using the same SD card, several times.
  • I can build my simple baremetal app in Vitis and boot it over JTAG, as well as QSPI, which works fine. Attempting to boot from SD with FSBL debug messaging enabled, I get:
    • SD: Unable to open file 1:/BOOT.BIN: 3, XFSBL_ERROR_SD_F_OPEN
  • I also have an Ultra96v2. Using the same SD card, I can boot a simple u96 baremetal app from the SD card on the u96.
  • The SD card is a 16GB delkin. I format it FAT and copy my BOOT.bin to it, simple.

Everything works fine on the U96, and the ZUB, except SD boot from the ZUB only. This is very strange and I can't figure what the issue could be. Any ideas?

  • Sign in to reply
  • Cancel

Top Replies

  • iksevas
    iksevas over 1 year ago in reply to tony56887 +2
    I have heard stories of 16Gb cards not functioning on some boards but 8Gb cards working fine. I have heard stories of different manufacturers working better than others. So, I would not be surprised if…
  • tony56887
    tony56887 over 1 year ago in reply to adielement +1 suggested
    Solved yesterday. This was a tools issue on version 2023.2 on interface SD1. SD0 works fine as that's what ultra96 is targeting. Version 2024.2 has this fixed.
Parents
  • Aymen
    0 Aymen over 1 year ago

    Hi tony,

    You mentioned successfully booting a baremetal app from the SD card on the Ultra96v2. I'm trying to do the same thing, but I'm running into issues. I've created a BOOT.BIN that includes the FSBL, bitstream, and my baremetal application. I've also set the boot mode to SD, but it doesn't seem to boot at all.

    Would you mind sharing a bit more about how you set it up on the U96? For example, how you formatted the SD card, where exactly you placed the BOOT.BIN, and if there were any special steps you took in Vitis or when generating the FSBL?

    Any help would be greatly appreciated!

    Thanks in advance.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • tony56887
    0 tony56887 over 1 year ago in reply to Aymen

    What you listed is what I did that worked on u96.

    Using vivado/vitis version 2023.2. In vitis once you have your platform and app developed and verified booting over jtag, select your app and click the 'create boot image'. FSBL and your app elf should already be listed, add your bitstream. Leave all other settings default. Select output path for bif and image.

    Format SD card FAT32 using host PC, I'm using ubuntu - Disks utility. Simply copy boot.bin right into the SD card. Set boot switch to SD. This process worked fine for me on u96.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • tony56887
    0 tony56887 over 1 year ago in reply to Aymen

    What you listed is what I did that worked on u96.

    Using vivado/vitis version 2023.2. In vitis once you have your platform and app developed and verified booting over jtag, select your app and click the 'create boot image'. FSBL and your app elf should already be listed, add your bitstream. Leave all other settings default. Select output path for bif and image.

    Format SD card FAT32 using host PC, I'm using ubuntu - Disks utility. Simply copy boot.bin right into the SD card. Set boot switch to SD. This process worked fine for me on u96.