Azure Sphere Module
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Azure Sphere Module
  • More
  • Cancel
Azure Sphere Module
Forum Development and production programmers for AES-MS-MT3620-M-G-2-TR
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Azure Sphere Module to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 3 subscribers
  • Views 2127 views
  • Users 0 members are here
  • azuresphmod
Related

Development and production programmers for AES-MS-MT3620-M-G-2-TR

pjschoenke
pjschoenke over 5 years ago

Hello!  One of my customers is developing a product with the Avnet Azure Sphere module: AES-MS-MT3620-M-G-2-TR

What would be the recommended programmers for development and debug initially and then for production of a product for 5000+/year?

Any feedback or input is welcomed and appreciated!

Thanks in advance!

Paul

  • Sign in to reply
  • Cancel
  • bwilless
    0 bwilless over 5 years ago

    Hi Paul,

     

    Sorry I did not see this question earlier.  The most direct path to developing a product that will leverage the Avnet Azure Sphere Module is to use the Avnet Azure Sphere Starter Kit.  The Starter Kit uses the same Azure Sphere Module, and code developed on the Starter Kit can run on the final production unit (assuming you use the same hardware interfaces) with zero changes.  Additionally, the Starter Kit has flexible expansion slots that make connecting external sensors and other hardware easy to accomplish.

     

    Check out our Blog with all the Avnet Azure Sphere content here on E14:  Avnet Azure Sphere Resources | element14 | Azure Sphere

     

    Let me know if I can help in any way,

    Brian

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • pjschoenke
    0 pjschoenke over 5 years ago in reply to bwilless

    Thanks Brian!  That helps and is appreciated!

    Can you elaborate more on a suggested solution for a production programmer?  Our customer is looking to do about 25K/year of these in production.

    Thanks again!

    Paul

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • bwilless
    0 bwilless over 5 years ago in reply to pjschoenke

    When you're planning your Azure Sphere production work flow you need to plan for manufacturing tasks/tests that require accessing the Azure Sphere device from a Windows10 PC.  The Azure Sphere PC software tools require the use of a USB-to-UART interface chip that exposes these interfaces to a PC in a way that allows the tools to recognize and interact with the Azure Sphere device.  Additionally, these tools require that the interface be implemented with the FTDI T4232HQ UART-to-USB interface chip. Microsoft has some documentation on this interface here.

     

    There are two approaches to consider . . .

     

    Approach #1: Include the FTDI device on your final product

     

    With this approach the FTDI interface is included on the final production unit.  The connector could be external to the unit or hidden inside the unit.

     

    Pros:

    • Provides the interface for production activities
    • Provides the interface for field technicians if needed

     

    Cons:

    • Adds BOM cost for all units
    • Exposes the interface for non-authorized technicians
      • Note unless the user had access to the devices Azure Sphere Tenant, there not much they could do with the unit other than wipe it clean or manage wifi networks.

     

    Approach #2: Provide connectivity (connector/socket) on the product for an external FTDI programming board

     

    Pros:

    • Reduces BOM cost for all units
    • Does not expose the interface for non-authorized technicians, of course clever engineers will always find a way!

     

    Cons:

    • Requires additional board design with FTDI device and some type of interface cable or socket to connect to production units

     

    Alternative approach

     

    I guess you could also develop a test fixture that you could drop one of the Avnet Azure Sphere modules into that connects to the correct pins to connect a FTDI device on the test fixture.  I don't see this as a preferred option because you'll want to run functional tests on your final production units so you would likely still need to implement one of the first two approaches.