Documentation   Reference Designs

 

The UltraZed-EV Carrier Card supports the UltraZed-EVTm System-on-Module (SOM), providing easy access to the full 152 user I/O, 26 PS MIO, 4 PS GTR transceivers, and 16 GTH transceivers available from the UltraZed-EV SOM via three Micro Headers. Two 200-pin Micro Headers on the carrier card mate with the UltraZed-EV SOM, connecting 152 of the UltraZed-EV Programmable Logic (PL) I/O along with 16 GTH transceivers to FMC HPC slot, LVDS Touch Panel interface, SFP+ interface, HDMI In/Out, 3G-SDI In/Out, push button switches, DIP switches, LEDs, Xilinx SYSMON, clock generators, and 2 Digilent PmodTm compatible interfaces.

 

The UltraZed-EV Carrier Card also uses a 120-pin Micro Header to gain access to the UltraZed-EV SOM Processing System (PS) MIO and GTR transceiver pins as well as USB 2.0 and Gigabit Ethernet interfaces. The UltraZed-EV SOM PS MIO and GTR pins are used on the UltraZed-EV Carrier Card to implement the microSD card, PMOD, USB 2.0/3.0, Gigabit Ethernet, SATA host, Display Port, PCIe Root Port, dual USB-UART, user LED and switch, and MAC Address device interfaces. The UltraZed-EV Carrier Card also provides several power rails to the UltraZed- EV SOM including the 12V main input voltage, user selectable bank voltages for the PL I/O (VCCOs), and the necessary voltages for the GTR and GTH transceivers. The UltraZed-EV Carrier Card is a great vehicle for validating the UltraZed-EV SOM and provides an excellent starting point for creating your own UltraZed-EV custom carrier card.

 

First shipments of the UltraZed-EV Carrier Card will be included in the UltraZed-EV Starter Kit, with delivery expected mid-summer 2018.

 

TopBackFrontAngleAngle

image

image

image

image

image

 

Reference Designs

SDSoC Baremetal Platform - Xilinx Matrix Multiply Example

SDSoC_Platform_v2018

SDSoC_Platform_v2018.3

 

SDSoC PetaLinux Platform - Xilinx Matrix Multiply Example

UltraZed-EV SDSoC Platform v2018.2

 

UltraZed-EV Master User Constraint List

UltraZed-EV-CC-Master-XDC_0.zip

 

UltraZed-EV Ethernet Performance Test Tutorial
Zynq UltraScale+ Measure networking performance when using an embedded operating system on the Avnet UltraZed-EV SOM + EV Carrier development board.

UltraZed-EV-RD_Ethernet_Performance_Test.zip

 

UltraZed-EV SATA Performance Test Tutorial
Description: Zynq UltraScale+ SATA drive read/write performance tests on the Avnet UltraZed-EV SOM + EV Carrier development board.

UltraZed-EV-RD-SATA_Performance.zip

 

Out-of-Box Designs Ultrazed-EV Carrier Card
This is the software and hardware platform, boot files, Linux kernel and RAMdisk that are provided on the pre-installed SD card.

uz7ev_evcc_sd_oob_2017_4_bsp.zip

 

PetaLinux Board Support Packages
Compressed PetaLinux BSPs for Avnet Zynq system platforms.

UltraZed-EV Carrier Card - PetaLinux 2020+ BSP (Sharepoint site)

UltraZed-EV Carrier Card – PetaLinux 2018.2 Standard BS

UltraZed-EV Carrier Card – PetaLinux 2018.2 Enhanced BSP

UltraZed-EV Carrier Card – PetaLinux 2017.4 Standard BSP

 

Vitis PetaLinux Platform

UltraZed-EV Carrier Card - Vitis Platform 2020+ (Sharepoint site)

 

Vitis PetaLinux Platform PreBuilt Example

UltraZed-EV Carrier Card - Vitis PetaLinux Platform 2020+ Vector Add (Sharepoint site)

 

Development Using Ubuntu Desktop Linux
These tutorials provide a means to integrate several different technologies on a single platform.  Using the Avnet target boards, we have the power of ARM processors, combined with the unrivaled flexibility of Xilinx programmable logic to implement custom hardware systems.    We use a Linux kernel as the foundation operating system running on the processor cores which enables a very large ecosystem of software to be run on our development kits. Virtual machines can provide a very convenient Ubuntu development environment for building the hardware platform and cross-compiling software to target the Processing System.

VirtualBox and Linux VM Installation Guide v2020+ (Sharepoint site)

VirtualBox and Linux VM Installation Guide v2016.4

VirtualBox and Linux VM Installation Guide v2017.1

VirtualBox and Linux VM Installation Guide v2017.2

VirtualBox and Linux VM Installation Guide v2018.2

VirtualBox and Linux VM Installation Guide v2018.3

 

 

WHAT'S INCLUDED
  • UltraZed-EV Carrier Card
  • 12V AC/DC Power Supply
  • Quick Start Card
  • microUSB Cable
  • UltraZed-EV SOM Mounting Hardware
  • microSD Card 8GB
  • RJ45 Cable
Related Blog Posts
  • Homestretch To Production - MAC Address Programming Approaches

    Introduction When running a race the homestretch refers to an area between the last turn and the winning post.  It can also refer to the last part of a product design project or a new production release campaign.  In each case, partici...
  • Use MATLAB to Debug your SoC IP Core

    Recently I discovered a clever way in MATLAB to interact with my HDL IP cores in situ, running in the programmable logic. Yes, of course, there are many ways to probe logic in an FPGA, but this one is particularly helpful when I need to analyze bits …