EXPLORE-NFC
  • Products & Partners
  • Dev Tools
  • EXPLORE-NFC
  • More
  • Cancel
EXPLORE-NFC
Forum Webinar: Basics of running NFC and RFID on your Raspberry Pi - 4/8/2015 9:00AM CDT (America/Chicago)
  • Blog
  • Forum
  • Documents
  • Events
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join EXPLORE-NFC to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 7 replies
  • Subscribers 11 subscribers
  • Views 1132 views
  • Users 0 members are here
  • access
  • raspberry
  • b+
  • pi
  • control
  • rfid
  • explore-nfc
  • raspberrypi
  • nfc
  • webinar
  • nxp
Related

Webinar: Basics of running NFC and RFID on your Raspberry Pi - 4/8/2015 9:00AM CDT (America/Chicago)

elau
elau over 11 years ago

Join the webinar and learn about the basics of NFC, modes of operation, communication protocols and the new scenarios that the technology opens in the contactless applications domain. The second half of the webinar will be used to demonstrate use cases that can be realized with the expansion board for the Raspberry Pi.

 

Register NOW!

http://www.element14.com/community/events/4277

 

When and Where

  • Start Time: 4/8/2015 9:00 AM CDT (America/Chicago)

  • End Time: 4/8/2015 10:00 AM CDT (America/Chicago)

  • Location: Online - Webex

 

To learn more or purchase the EXPLORE-NFC expansion board for the Raspberry Pi used in this webinar:

Please visit: http://www.element14.com/community/community/designcenter/explorenfc

  • Sign in to reply
  • Cancel

Top Replies

  • michaelneurohr
    michaelneurohr over 11 years ago +1
    You can download yesterdays slides from here: https://nxp.box.com/ExploreNFCWebinar Michael
Parents
  • packetgeek
    packetgeek over 11 years ago

    Since the board is designed for the Raspberry Pi, I'm assuming that the board doesn't have the pull-up resistors (they're on the Pi).  If we were to use the board with a different controller that didn't have the resistors, we'd have to add them (possibly a level converter too).  Anyone have any recommended values for the resistors?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • packetgeek
    packetgeek over 11 years ago

    Since the board is designed for the Raspberry Pi, I'm assuming that the board doesn't have the pull-up resistors (they're on the Pi).  If we were to use the board with a different controller that didn't have the resistors, we'd have to add them (possibly a level converter too).  Anyone have any recommended values for the resistors?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • michaelneurohr
    michaelneurohr over 11 years ago in reply to packetgeek

    Not sure which one you mean.

    Reset pin and I2C do have pull up in place. For SPI it's not needed.

    IRQ pin does not have one in place.

    But most MCUs have built in pull-up and pull-down resistors.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • packetgeek
    packetgeek over 11 years ago in reply to michaelneurohr

    That's good to know.  I'd asked about the resistors because I've been working with Arduino boards on the Raspberry Pi.  Arduinos don't have the resistors as they're normally place on the boards.  In some cases, it's not a problem.  In others, the I2C interface won't function.  Thanks in any case.

     

    - Tim