EXPLORE-NFC
  • Products & Partners
  • Dev Tools
  • EXPLORE-NFC
  • More
  • Cancel
EXPLORE-NFC
Forum Error building the library Neardal
  • Blog
  • Forum
  • Documents
  • Events
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join EXPLORE-NFC to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 7 replies
  • Subscribers 10 subscribers
  • Views 1121 views
  • Users 0 members are here
Related

Error building the library Neardal

e14 Contributor
e14 Contributor over 11 years ago

Hi All,

 

I tried all the different solutions available for building the library neardal. Everytime I face the same error.

 

make  all-recursive

make[1]: Entering directory '/home/pi/Source/neardal-master'

Making all in lib

make[2]: Entering directory '/home/pi/Source/neardal-master/lib'

Makefile:422: warning: overriding recipe for target '.dirstamp'

Makefile:396: warning: ignoring old recipe for target '.dirstamp'

Makefile:425: warning: overriding recipe for target '.deps/.dirstamp'

Makefile:399: warning: ignoring old recipe for target '.deps/.dirstamp'

Makefile:484: .deps/libgenerated_la-dbus-object-manager.Plo: No such file or directory

Makefile:485: .deps/libgenerated_la-dbus-properties.Plo: No such file or directory

Makefile:486: .deps/libgenerated_la-neard_adapter_proxy.Plo: No such file or directory

Makefile:487: .deps/libgenerated_la-neard_manager_proxy.Plo: No such file or directory

Makefile:488: .deps/libgenerated_la-neard_tag_proxy.Plo: No such file or directory

Makefile:489: .deps/libgenerated_la-neardal_agent.Plo: No such file or directory

Makefile:490: .deps/neardal.Plo: No such file or directory

Makefile:491: .deps/neardal_adapter.Plo: No such file or directory

Makefile:492: .deps/neardal_agent_mgr.Plo: No such file or directory

Makefile:493: .deps/neardal_device.Plo: No such file or directory

Makefile:494: .deps/neardal_manager.Plo: No such file or directory

Makefile:495: .deps/neardal_record.Plo: No such file or directory

Makefile:496: .deps/neardal_tag.Plo: No such file or directory

Makefile:497: .deps/neardal_tools.Plo: No such file or directory

Makefile:498: .deps/neardal_traces.Plo: No such file or directory

make[2]: *** No rule to make target '.deps/neardal_traces.Plo'.  Stop.

make[2]: Leaving directory '/home/pi/Source/neardal-master/lib'

Makefile:411: recipe for target 'all-recursive' failed

make[1]: *** [all-recursive] Error 1

make[1]: Leaving directory '/home/pi/Source/neardal-master'

Makefile:296: recipe for target 'all' failed

make: *** [all] Error 2

 

 

 

Can some one please help me with this , or can you please list down the steps that you followed to install the library.

 

Thanks,

Mohit

  • Sign in to reply
  • Cancel
  • clem57
    clem57 over 11 years ago

    Did you follow this? https://github.com/connectivity/neardal

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to clem57

    Hey Clem,

     

    Ya i followed the exact procedure

    1) ./autogen.sh

    2) ./configure

    3) make

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago

    I encountered this exact problem.  I solved it by:

    - deleted the "neardal" directory in which I had run "make" to cause this problem

    - fetched the neardal tarball again with "wget https://github.com/connectivity/neardal/archive/0.14.tar.gz"

    - uncompressed the tarball with by double clicking it in the GUI file manager, creating the "neardal-0.14" directory

    - then typed these commands into a shell window:

    cd neardal-0.14

    ./autogen.sh

    ./configure --prefix=/usr --sysconfdir=/etc --localstatedir=/var

    make

    sudo make install

    Everything went nicely, this  time.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to e14 Contributor

    Hello,

    Thank you Ed Boakes,for your solution! All of that helped me.

    However once that I launch "./ncl" I've:

     

    root@raspberrypi:/home/pi/neardal-0.14/ncl# ./ncl

    Compiled at May  9 2015 : 02:28:10

     

    Segmentation fault

     

    I've folowinf this :

    Testing

    =======

    Compile neardal and get Neard running.

    under ncl directory (ncl:Neardal Command Line) run:

     

    ./ncl

     

    This command line interpretor include a set of the main commands use to test neardal/Neard.

     

     

    I would like use my NXP - EXPLORE-NFC for raspberry pi and to be able to read the proprities and the content of tag in order to write on it.

     

    Someone could he help me please ?

    Because Element14 in their "Quick Start-up Guide" mention only to: "Programming tags : To program tags quickly, you can use the NXP TagWriter app for Android:"

    That not possible to write with the card ?

    I buy this tool to do that.

    Please help me

     

    Thanks Axel

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to e14 Contributor

    Hi Axel,

     

    Never seen your previous problem but could you re-sync and retry please?

     

    just

     

    ./autogen.sh

    make

    would be enough. You can execute the command line tool localy (ncl/ncl), avoiding a make install, or try the demo binary (used as sample code), with demo/demo.

     

    Hope this help,

    Frederic

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • flashback
    flashback over 11 years ago in reply to e14 Contributor

    SOLVED --> look @ next post

     

    Hi Frederic, i'm trying to compile too, but this time for Kali linux for raspberry 2, and i'm stuck here:

    .....

    configure: NEARDAL will be compiled in C99 mode

    configure: NEARDAL will be compiled with -Wpedantic

    configure: NEARDAL will be compiled with CFLAGS=-g -O2

    configure: NEARDAL will be compiled with extra flags NEARDAL_EXTRA_FLAGS=-Wpedantic

    checking for a sed that does not truncate output... (cached) /bin/sed

    ./configure: line 11648: syntax error near unexpected token `gio,'

    ./configure: line 11648: `PKG_CHECK_MODULES(gio, gio-unix-2.0 >= 2.30,'

     

    could you please help me to find out which lib is actually missing ?

    i already tried installing:

    libgio-cil - CLI binding for the GIO I/O stack 2.22

    libgio2.0-cil-dev - CLI binding for the GIO I/O stack 2.22

    libgio3.0-cil - CLI binding for the GIO libraries 2.24

    libgio3.0-cil-dev - CLI binding for GIO 2.24

    but none of that worked (in fact all are version <= 2.30)

    Any hint would be welcome !

    Thanks in advance.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • flashback
    flashback over 11 years ago in reply to flashback

    I was wrong, searching for the wrong libs, by the way, i solved it with:

    apt-get install libgtkgl2.0-dev