EXPLORE-NFC
  • Products & Partners
  • Dev Tools
  • EXPLORE-NFC
  • More
  • Cancel
EXPLORE-NFC
Forum PIN Connection to PI
  • Blog
  • Forum
  • Documents
  • Events
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join EXPLORE-NFC to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 4 replies
  • Answers 1 answer
  • Subscribers 9 subscribers
  • Views 1339 views
  • Users 0 members are here
Related

PIN Connection to PI

e14 Contributor
e14 Contributor over 10 years ago

Please provide a specification which of the pins need actually be connected for the NFC reader in it's default configuration (SPI). I would like to connect another addon that is based on the UART, which is not used but within the 26 PIN header blocked by the NFC reader.

 

Thanks.

  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    found in sw3693\linux\shared\phhwConfig.h

    #ifdef NXPBUILD__PHHAL_HW_RC523 //Explore-NFC board

     

    #if BOARD == RaspberryPi_Rev1_Pinout

    #define SPI_CONFIG           "0:0:0" //PN512 is connected to SPI bus 0, CS pin 0, no busy pin

    #define PIN_CS_IN           0

    #define PIN_IRQ               23

    #define PIN_NRST           7

     

     

    #elif BOARD == RaspberryPi_Rev2_Pinout

    #define SPI_CONFIG           "0:0:0" //PN512 is connected to SPI bus 0, CS pin 0, no busy pin

    #define PIN_CS_IN           2

    #define PIN_IRQ               23

    #define PIN_NRST           7

     

     

    #endif

     

    #endif /* NXPBUILD__PHHAL_HW_RC523 */

     

    # during initialisation directions are set

    ret = gpio_set_direction(PIN_CS_IN, false);

    ret = gpio_set_direction(PIN_IRQ, false);

    ret = gpio_set_direction(PIN_NRST, true);

    • SPI: 19,21,23,24 (CS0)
    • PIN_CS_IN 2 (BCM numbering)
    • PIN_NRST 7 (BCM numbering)
    • Does it use 3.3V power only or also 5V?

    Is that correct? Can someone tell if PIN_CS_IN and PIN_NRST use the wiring PIN numbering (and would then map to GPIO2 / physical 13, GPIO7 / physical 7?

    > from the schematic below the numbers used in the code are BCM

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 10 years ago in reply to e14 Contributor

    Hi Max,

     

    I don't have this board but there is a full schematic here, you can see the 26-way connector at the bottom, marked with all signals and voltages.

    EXPLORE NFC Board Schematic

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to shabaz

    Perfect. I'll find out if it works with it's i2c lines not conneted.