EXPLORE-NFC
  • Products & Partners
  • Dev Tools
  • EXPLORE-NFC
  • More
  • Cancel
EXPLORE-NFC
Forum Compile Examples
  • Blog
  • Forum
  • Documents
  • Events
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join EXPLORE-NFC to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 15 replies
  • Subscribers 10 subscribers
  • Views 2751 views
  • Users 0 members are here
Related

Compile Examples

e14 Contributor
e14 Contributor over 11 years ago

Hello,

Firstly I would like to say sorry that I´m a very big noob at C programming, because I never did this before.

I had a look at the examples today and customised them a little bit. How do I compile the C files in order to run them now? I´m sure that cc -o basic basic.c is the wrong solution. I´m sure that the answer is very easy but as I´ve already mentioned I´m totally unexperienced with C, so please forgive me image

 

Thank you very much in advance.

  • Sign in to reply
  • Cancel

Top Replies

  • michaelneurohr
    michaelneurohr over 11 years ago in reply to clem57 +1
    Hi Clem, the LPCXpresso IDE is only used for the software projects running on the MCUs LPC1769 and LPC1227. For the Raspberry Pi projects please build on the Raspberry Pi directly. Michael
  • e14 Contributor
    e14 Contributor over 11 years ago +1
    Of course. Firstly I´ve installed all libraries and extensions provided in the README.md file and afterwards I ran the following commands in the root folder of the source files: ./bootstrap ./configure…
  • clem57
    0 clem57 over 11 years ago

    I am going to guess you have Linux. If so look for gcc or better yet the example may have a file called makefile. If so run "make" should do the dirty work. Be careful not to overwrite something important! If you really feel new, please list what you found where it came from and I can try it for myself and help.

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to clem57

    Hello Clem,

    Thanks for your response.

    Correct. I´m using Debian (Raspbian). Well I´ve downloaded the sourcecode of the sample file available here on the site (http://www.nxp.com/documents/software/SW282814.zip) and then I went to the /examples folder, made some changes to the basic.c file and tried to compile it afterwards.

     

    I´ve already tried "make" and I got the following response:  make: *** No targets.  Stop.

    You can find the content of my makefile here: http://pastebin.com/7aJPN3u1

     

    When I try the gcc one I get the same error like when I do it with cc:

    basic.c:18:18: fatal error: glib.h: No such file or directory

    compilation terminated.


    Any ideas?

    Thank you very much in advance,

    Lukas.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • clem57
    0 clem57 over 11 years ago in reply to e14 Contributor

    The accompanying sample applications can be compiled along with the library and runs

    on the LPC1769 board attached with either the PN512 or the CLRC663 blue board. This

    compilation of the project is tested on Microsoft Windows 7 64-bit Operating System

    using the LPCXpresso IDE mentioned above.

    You need to install LPCXpresso IDE on Windows 7 preferably(maybe only choice). I will bet they have how to import and compile this there.

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • michaelneurohr
    0 michaelneurohr over 11 years ago

    In the source files you should find a README file with step by step instructions about how to compile the sources.

    The easiest would be to compile directly on the Raspberry Pi. Otherwise you would need a cross toolchain.

     

    Let me know if that helps.

     

    Michael

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • michaelneurohr
    0 michaelneurohr over 11 years ago in reply to clem57

    Hi Clem,

     

    the LPCXpresso IDE is only used for the software projects running on the MCUs LPC1769 and LPC1227.

    For the Raspberry Pi projects please build on the Raspberry Pi directly.

     

    Michael

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to michaelneurohr

    Hi Michael,

    I´ve done all steps mentioned in the README.md file and it worked fine. Thank you very much! Sorry for my own stupidity, I should just read all documentation files next time.

    But now I have another question. How do I get the tag UID? I´m using the default tag which was included in the package, but I get no UID output.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • clem57
    0 clem57 over 11 years ago in reply to e14 Contributor

    Fantastic! Can you share what changes you made?

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    Of course.

    Firstly I´ve installed all libraries and extensions provided in the README.md file and afterwards I ran the following commands in the root folder of the source files: ./bootstrap ./configure and make. Then it compiled everything and it also made a makefile in the examples/ directory. Now I can compile the examples directly in the examples directory by just entering make.

    Thanks to you two again for your help. The only thing I still need to get working now is to get the UID of the card image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • michaelneurohr
    0 michaelneurohr over 11 years ago in reply to e14 Contributor

    Hi,

    I'm glad you got it working.

     

    We added UID support to the basic example later on. Because of that please make sure to use the latest version from [1]. There was an update just three days ago. Please also make sure to update libneardal too.

     

    Michael

     

    [1] EXPLORE-NFC - Exclusive from element14 :: NXP Semiconductors

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to michaelneurohr

    Hi,

    Ah okay thanks. I´ve installed the new version and afterwards I got the following output:

     

    Waiting for tag or device...

    on_name_lost() : :org.neardal

    Found record /org/neard/nfc0/tag0/record0

    Record type: Text

    URI: 

    Title: Example

    Action: 

    Language: en

    Encoding: UTF-8

    Segmentation fault


    My libneardal is up to date (Version 0.14.2-1) and I´m using the lastest example, but I only get "Segmentation fault" and no UIDs of the card(s).


    Thanks,

    Lukas


    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
>