EXPLORE-NFC
  • Products & Partners
  • Dev Tools
  • EXPLORE-NFC
  • More
  • Cancel
EXPLORE-NFC
Forum Building ExploreNFC from source on Raspbian Jessie image 2017-06-21
  • Blog
  • Forum
  • Documents
  • Events
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join EXPLORE-NFC to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 1 reply
  • Subscribers 8 subscribers
  • Views 818 views
  • Users 0 members are here
  • explore-nfc
  • raspberry explore-nfc
  • raspbian jessie
Related

Building ExploreNFC from source on Raspbian Jessie image 2017-06-21

noeldkendall
noeldkendall over 9 years ago

Environment:

Pi Systems: Raspberry Pi 3 Model B (revision a22082) and Raspberry Pi Model B Rev 2 (revision 000e)

NXP Explorer Board (element14) Explore-NFC Rev 1.6

 

I am trying to build from source for both reference and I have a proof of concept project (part of a much larger project)

and need to develop some custom handling.

 

According to the current links (as of time of posting) from NXP website, I need the following archive files:

SW282816.zip

SW3639.zip

 

I am familiar with C and both read and code in it, but these are dusty skills, although in the past I have succeeded at

developing device drivers. Just to level set abilities. I am these days a Java Enterprise developer. My POC goal is to

build a Tomcat webapp that will on demand prepare the reader to receive information from an Android Kitkat+ device via

NFC. A step along the way will be do build out a Java JNI wrapper around access to the NXP board. The explorer examples

will act as a reference to determine what is needed in this JNI wrapper.

 

I don't see an archive for a compatible version of neardal - hence I fetched 0.14-3.tar.gz from github AppNearMe archives.

The resulting package builds without error. I am unsure if this code is compatible or not, which adds to my confusion. My understanding

is that this is the component that will interface with dbus. I see that the installation implants /etc/dbus-1/system.d/org.neard. This configuration

file is slightly different than the one which is installed using the .deb files out of SW2827.zip. 2827 installs

 

 

Following the instructions in document AN11802.pdf, I have attempted to build what is needed from source. There are some issues

I am having difficulty resolving.

 

1) SW3639 is the NxpNfcRdLib. I encounter compile errors in NfcrdlibEx5_ISO15693 as follows:

 

[ 87%] Building C object NfcrdlibEx5_ISO15693/CMakeFiles/NfcrdlibEx5_ISO15693.dir/NfcrdlibEx5_ISO15693.c.o
/Volumes/workvol/workspaces/raspbian/work/NxpNfcRdLib-201708221632/NfcrdlibEx5_ISO15693/NfcrdlibEx5_ISO15693.c: In function ‘NfcrdlibEx5_ISO15693’:
/Volumes/workvol/workspaces/raspbian/work/NxpNfcRdLib-201708221632/NfcrdlibEx5_ISO15693/NfcrdlibEx5_ISO15693.c:209:43: error: ‘phacDiscLoop_Sw_DataParams_t’ has no member named ‘sTypeVTargetInfo’
                 phApp_Print_Buff(sDiscLoop.sTypeVTargetInfo.aTypeV[0].aUid, 0x08);
                                           ^
/Volumes/workvol/workspaces/raspbian/work/NxpNfcRdLib-201708221632/NfcrdlibEx5_ISO15693/NfcrdlibEx5_ISO15693.c:212:47: error: ‘phacDiscLoop_Sw_DataParams_t’ has no member named ‘sTypeVTargetInfo’
                 memcpy(aReceivedUid, sDiscLoop.sTypeVTargetInfo.aTypeV[0].aUid, 0x08);
                                               ^
/Volumes/workvol/workspaces/raspbian/work/NxpNfcRdLib-201708221632/NfcrdlibEx5_ISO15693/NfcrdlibEx5_ISO15693.c:215:50: error: ‘phacDiscLoop_Sw_DataParams_t’ has no member named ‘sTypeVTargetInfo’
                 if (DisplayCardTypeInfo(sDiscLoop.sTypeVTargetInfo.aTypeV[0].aUid) == PH_ERR_SUCCESS)
                                                  ^
/Volumes/workvol/workspaces/raspbian/work/NxpNfcRdLib-201708221632/NfcrdlibEx5_ISO15693/NfcrdlibEx5_ISO15693.c:226:62: error: ‘salI15693’ undeclared (first use in this function)
                         status = phalI15693_ReadSingleBlock(&salI15693,
                                                              ^
/Volumes/workvol/workspaces/raspbian/work/NxpNfcRdLib-201708221632/NfcrdlibEx5_ISO15693/NfcrdlibEx5_ISO15693.c:226:62: note: each undeclared identifier is reported only once for each function it appears in
/Volumes/workvol/workspaces/raspbian/work/NxpNfcRdLib-201708221632/NfcrdlibEx5_ISO15693/NfcrdlibEx5_ISO15693.c:227:29: error: ‘PHAL_I15693_OPTION_OFF’ undeclared (first use in this function)
                             PHAL_I15693_OPTION_OFF,
                             ^
/Volumes/workvol/workspaces/raspbian/work/NxpNfcRdLib-201708221632/NfcrdlibEx5_ISO15693/NfcrdlibEx5_ISO15693.c:286:26: error: ‘PHPAL_SLI15693_FLAG_NBSLOTS’ undeclared (first use in this function)
                         (PHPAL_SLI15693_FLAG_NBSLOTS | PHPAL_SLI15693_FLAG_DATA_RATE | PHPAL_SLI15693_FLAG_INVENTORY),
                          ^
/Volumes/workvol/workspaces/raspbian/work/NxpNfcRdLib-201708221632/NfcrdlibEx5_ISO15693/NfcrdlibEx5_ISO15693.c:286:56: error: ‘PHPAL_SLI15693_FLAG_DATA_RATE’ undeclared (first use in this function)
                         (PHPAL_SLI15693_FLAG_NBSLOTS | PHPAL_SLI15693_FLAG_DATA_RATE | PHPAL_SLI15693_FLAG_INVENTORY),
                                                        ^
/Volumes/workvol/workspaces/raspbian/work/NxpNfcRdLib-201708221632/NfcrdlibEx5_ISO15693/NfcrdlibEx5_ISO15693.c:286:88: error: ‘PHPAL_SLI15693_FLAG_INVENTORY’ undeclared (first use in this function)
                         (PHPAL_SLI15693_FLAG_NBSLOTS | PHPAL_SLI15693_FLAG_DATA_RATE | PHPAL_SLI15693_FLAG_INVENTORY),
                                                                                        ^

All other code out of this project builds correctly. There is a resulting NxpNfcRdLib.a built without error, as well as the other examples.

 

2) SW282816 will not complete the cmake step.  The CMakeFiles.txt at project top references an external project to build the NxpNfcRdLib. The cmake terminates when

it discovers the needed external project (which defaults to a subfolder of the project) is empty. I would rather not monkey around with the cmake file as my working style

is to build shell scripts that will idempotently build the artifacts needed - and sed'ing the CMakeFiles is not a fun coding exercise (but I will do it if I have to).

 

The relevant results of the cmake are:

 

CMake Error at /usr/share/cmake-3.6/Modules/ExternalProject.cmake:1924 (message):

  No download info given for 'NXPRDLIBLINUX' and its source directory:

 

 

   /Volumes/workvol/workspaces/raspbian/work/NxpNfcRdLib-201708221632/nxprdlib-linux

 

 

  is not an existing non-empty directory.  Please specify one of:

 

 

   * SOURCE_DIR with an existing non-empty directory

   * URL

   * GIT_REPOSITORY

   * HG_REPOSITORY

   * CVS_REPOSITORY and CVS_MODULE

   * SVN_REVISION

   * DOWNLOAD_COMMAND

Call Stack (most recent call first):

  /usr/share/cmake-3.6/Modules/ExternalProject.cmake:2473 (_ep_add_download_command)

  CMakeLists.txt:13 (ExternalProject_Add)

 

 

 

 

-- Checking for module 'glib-2.0>=2.40'

--   Found glib-2.0, version 2.42.1

-- Checking for module 'gthread-2.0>=2.40'

--   Found gthread-2.0, version 2.42.1

-- Checking for module 'gio-2.0>=2.40'

--   Found gio-2.0, version 2.42.1

-- Checking for module 'gio-unix-2.0>=2.40'

--   Found gio-unix-2.0, version 2.42.1

-- Checking for module 'neardal'

--   Found neardal, version 0.14.0

-- Configuring incomplete, errors occurred!

See also "/Volumes/workvolworkspaces/raspbian/work/NFCExplorer-201708231321/neard-explorenfc-1.2/build/CMakeFiles/CMakeOutput.log".

makefile was not created - there was a cmake failure

 

3) Attempting to run neardal demo - I see 'no adapter found'

I have been sure to enable SPI on both Pi platforms, and lsmod shows:

Module                  Size  Used by

evdev                  12423  2

joydev                  9988  0

hidp                   15368  1

md4                     3862  0

md5                     2608  1

hmac                    3252  1

bnep                   12051  2

hci_uart               19956  1

btbcm                   7916  1 hci_uart

bluetooth             365511  27 hidp,hci_uart,bnep,btbcm

nls_utf8                1656  1

cifs                  421953  2

brcmfmac              222874  0

brcmutil                9092  1 brcmfmac

cfg80211              543027  1 brcmfmac

rfkill                 20851  4 bluetooth,cfg80211

snd_bcm2835            24427  1

snd_pcm                98501  1 snd_bcm2835

snd_timer              23904  1 snd_pcm

spidev                  7373  0

snd                    70032  5 snd_timer,snd_bcm2835,snd_pcm

i2c_bcm2835             7167  0

bcm2835_gpiomem         3940  0

spi_bcm2835             7596  0

uio_pdrv_genirq         3923  0

fixed                   3285  0

uio                    10204  1 uio_pdrv_genirq

i2c_dev                 6913  0

fuse                   99603  3

ipv6                  406751  58

 

Output from ./demo:

pi@pi3:/Volumes/workvol/workspaces/raspbian/work/NeardAl-201708230924/neardal-0.14-3/demo$ ./demo

 

 

neardal_mgr_prv_get_all_adapters(): Error: 2:GDBus.Error:org.freedesktop.DBus.Error.ServiceUnknown: The name org.neard was not provided by any .service files

 

In another terminal window, monitoring dbus, I see the following when I attempt to run the neardal demo:

 

pi@pi3:~$ dbus-monitor --system

signal sender=org.freedesktop.DBus -> dest=:1.28 serial=2 path=/org/freedesktop/DBus; interface=org.freedesktop.DBus; member=NameAcquired

   string ":1.28"

signal sender=org.freedesktop.DBus -> dest=(null destination) serial=42 path=/org/freedesktop/DBus; interface=org.freedesktop.DBus; member=NameOwnerChanged

   string ":1.29"

   string ""

   string ":1.29"

signal sender=org.freedesktop.DBus -> dest=(null destination) serial=43 path=/org/freedesktop/DBus; interface=org.freedesktop.DBus; member=NameOwnerChanged

   string ":1.29"

   string ":1.29"

   string ""

 

The dbus configuration file (which I did install using the .deb package) is as follows:

 

<!DOCTYPE busconfig PUBLIC

"-//freedesktop//DTD D-BUS Bus Configuration 1.0//EN"

"http://www.freedesktop.org/standards/dbus/1.0/busconfig.dtd">

<busconfig>

    <policy user="root">

        <allow own="org.neard"/>

        <allow send_destination="org.neard"/>

        <allow send_interface="org.neard.NDEFAgent"/>

        <allow send_interface="org.neard.PHDC.Manager"/>

        <allow send_interface="org.neard.PHDC.Agent"/>

        <allow send_interface="org.neard.HandoverAgent"/>

    </policy>

    <policy at_console="true">

        <allow send_destination="org.neard"/>

    </policy>

    <policy context="default">

        <allow send_destination="org.neard"/>

    </policy>

</busconfig>

 

 

I am reaching out to the community to see if anyone can help me straighten out this mess. The NXP board will not

react to any tag, including the standard MIFARE tag enclosed with the Explorer board from Element14.

  • Sign in to reply
  • Cancel
  • noeldkendall
    noeldkendall over 9 years ago

    Investigating the code further, example 5 appears to build out code that is not supported on the Pi. The build scripts seem not to take this into account, and attempts to build the example even though the #define switches in the header files do not result in inclusion of the necessary struct definitions.

     

    Commenting out the code using #ifdef for Pi builds, the module will build.

     

    However, the build proceeds to attempt an install, and no install target is found in NXPRDLIB.

     

    Stymied again.

     

    Can the correct artifacts (ZIP files) be placed under the software tab to correctly build the support for

    NXP-Explorer. It's a confusion as it stands.