MEMS Sensors Evaluation Board
  • Products & Partners
  • Dev Tools
  • MEMS Sensors Evaluation Board
  • More
  • Cancel
MEMS Sensors Evaluation Board
Forum Can this board be used with java?
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join MEMS Sensors Evaluation Board to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 3 replies
  • Subscribers 5 subscribers
  • Views 1622 views
  • Users 0 members are here
  • help
  • raspberrypi
  • sensor
  • java
Related

Can this board be used with java?

e14 Contributor
e14 Contributor over 12 years ago

Hi,

I am currently trying to write a little program in java which would display information from the sensors on the board, but I am struggling with how i would do this in java compared to the python scripts provided which use the sensor.so file to communicate with the board.

 

Many thanks

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 10 years ago

    The difference between a language like java (or c#) and a lower level language like c or c++ is the fact that they have a virtual machine. This has many advantages, like making the application platform-independent. But it also means that each platform has to have the vm for it.Now, microcontrollers are not uniform and vary in power, memory, and many other features. So adopting the JVM (java's virtual machine) for them is not easy even when possible. Most of the time its just impossible - most of the uc have very low memory capacity (part of what makes them cheap) - this would make fitting any general-purpose JVM there impossible, not to mention also with the application code.I am aware of some partial-implementations of java for microcontrollers. For example "java-based" sim cards (which have a very small controller inside) are there, but they have a very limited version of java.

    The memory usage shown is virtual memory used, not real memory... JVM just allocates a bunch when it starts.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 10 years ago

    The difference between a language like java (or c#) and a lower level language like c or c++ is the fact that they have a virtual machine. This has many advantages, like making the application platform-independent. But it also means that each platform has to have the vm for it.Now, microcontrollers are not uniform and vary in power, memory, and many other features. So adopting the JVM (java's virtual machine) for them is not easy even when possible. Most of the time its just impossible - most of the uc have very low memory capacity (part of what makes them cheap) - this would make fitting any general-purpose JVM there impossible, not to mention also with the application code.I am aware of some partial-implementations of java for microcontrollers. For example "java-based" sim cards (which have a very small controller inside) are there, but they have a very limited version of java.

    The memory usage shown is virtual memory used, not real memory... JVM just allocates a bunch when it starts.